Part Number: DS90UB947-Q1 Hi team,
The customer currently uses the dual PORT inputs of 947. LVDS shares a set of clock inputs. I understand that D0- and D0+ must be of equal length. On the same port, for example: Within what error do the trace lengths of…
Part Number: DS90UB947-Q1 Hi,
Please also help with the following questions. Thank you. How to set up the LVDS part?(As shown in the attachment). What parameters need to be modified in the I2C register part?
LVDS.rar
Part Number: DS90UB947-Q1 Other Parts Discussed in Thread: DLPC230-Q1 Hi,
I have two openLDI questions want to confirm:
1. I tjit listed in DS90UB947-Q1 datasheet (figure1) is the "input data position" defined in dlpc230-Q1 datasheet (figure2), right? as…
Jon,
I am not sure what you are trying to show here. Can you please respond to my previous inquiry?
Casey McCrea said: Can you please share a picture of the total setup as well as pictures of the top side markings of the 947 and 948?
Best Regards,
Cas…
Part Number: DS90UB947-Q1 hi Team,
SAIC EP39 project DMH model use 947+948, now receive SAIC back-end information, the vehicle during the customer use of the vertical line of projection screen problem;
Details are as follows: (1) The occurrence of malfunction…
Part Number: DS90UB947-Q1 Hi team,
For UB948 AC-coupling cap selection, how to understand below screenshot? Is it a typo, both items are for RIN[1:0]+?
For UB947, what should we do for Dout1- and Dout1+ if we only use 1 link FPD-LINK output and work…
Part Number: DS90UB947-Q1 Hi,
My IVI project design with ser 947 and des 940, 947and 940 only use SPI to communicate, no image need to transmit and no image input to 947. I use 947's internal clock for pclk,make 940 lock to 947.940 use for instrument…
Part Number: DS90UB947-Q1 Other Parts Discussed in Thread: DS90CF388A Im working with DS90UB947 serializer, looking to go from OPEN LDI to DS90UB947 to deseralizer to 24bit parallel? Would i need to use DS90UB947 to DS90UB948 to something like DS90CF388A…
Part Number: DS90UB947-Q1 Hi friends at TI
If I set the remote deserialiser into I2C pass through all mode can I listen in on the remote traffic going on on the other side of the device without upsetting any operation that side. I can see the local traffic…