Part Number: DS90UB948-Q1 Other Parts Discussed in Thread: DS90UB949-Q1 , Tool/software: Current FCE need TI technical team to provide new configuration file(registers values) based on these parameters
The Serializer is DS90UB949-Q1 and the Deserializer…
Hi Anis,
Thank you for sharing the block diagram and additional information.
We usually do not see low resolution fuzzy display issues. Patgen will allow us to deduce if the issue is from the deserializer or incoming video.
Anis AROUS said: Regarding…
Part Number: DS90UB949A-Q1 Other Parts Discussed in Thread: DS90UB948-Q1 , , DS90UH948-Q1 , DS90UH949A-Q1 Hi sir,
Below is DS90UB949A-Q1+DS90UB948-Q1 combination, is this application support > 10M distance? What's the maximum distance?
Is there…
Part Number: DS90UB948-Q1 Other Parts Discussed in Thread: DS90UB949-Q1 , Hi
Can DS90UB948-Q1 transmit I2S audio to DS90UB949-Q1 side ? (I2S from 948 to 949)
Part Number: DS90UB948-Q1 Tool/software: Hello team,
There is a ground short circuit at PIN2 CAP_I2S of the DS90UB948 during production, but customer production line's detection mechanism could not identify this issue, and the INT pin of the 948 was…
Part Number: DS90UB948-Q1 Hi E2E,
I have a question regarding the mode select table:
If I use the Dual OLDI output, the MAP_SEL can be setted 0 or 1. I noticed that the voltage and R1 R2 are different.
Are there any other differences? How should…
Part Number: DS90UB948-Q1 Tool/software: Hi team,
Tier 1:Harman
OEM: BAIC
As shown in the figure, STP mode, from the 948Spec only see AC Capacitor recommendations for the 925, 927, 947, 949, the current BJEV project is with the DS90UB941. DS90UB943…
Part Number: DS90UB948-Q1 Tool/software: Hi,
Does FPDLink III specify a recommended value for BER?
I was able to calculate the BER using the BIST function, but if there are standards indicating what target value I should aim for, please let me know…
Part Number: DS90UB948-Q1 Tool/software:
Hi,
There are various standards for high-speed signal communication. In addition to FPDLink, there are GMSL, GVIF, and Clocklesslink, among others. All of them use differential signals and have similar bps…
Part Number: DS90UB948-Q1 Tool/software: Hello there,
I'm looking for channel specs for FPD-III serdes DS90UB947 + DS90UB948, i.e. what is the link budget, what is the acceptable cross-talk, etc.
Per the thread interface-forum/913246/ds90ub948-q1…