Part Number: DS90UB953A-Q1 Tool/software: Hi,
Does ub953 support data transmission in this way?
camera1----->RX1- UB954- -----|
| ----mipi-->UB953-------->
camera2----->RX2 -- UB954-----|
Part Number: DS90UB953A-Q1 In DS90UB953A-Q1 data sheet, it mention that
1. FPD-Link III 4.16-Gbps Serializer with CSI-2 Interface for 2.3MP/60fps Cameras
2. D-PHY v1.2 and CSI-2 v1.3 compliant system interface Up to 4 data lanes at 832 Mbps per each…
Part Number: DS90UB953A-Q1 Tool/software: Hi,
We have a video card integerted with Des954,Ser953 and a FPGA inside.
The FPAG will copy all CSI data from Des954 to Ser953.
We want connect the video card between a camera with Ser913 and ECU with Des914…
Part Number: DS90UB953A-Q1 Tool/software: In some cases, i2c scl signal measured shown 100Khz when Local slave proxy Ti960 I2C set fast plus mode (1Mhz), remote mast proxy ti953 i2c set fast plus mode(1Mhz).
case 1. Just connect ti960 to host processor…
Part Number: DS90UB953A-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 Hi,
We are working on DS90UB953-Q1 for FPD-Link III interface in one of our ADAS testing tool development.
As this layout has been already reviewed by you as per the below link…
Part Number: DS90UB953A-Q1 Hello,
in extension to my former forum request ds90ub953a-q1-supported-csi-data-types I have the following question:
If the 953/954 just forward CSI packets, are there any restrictions regarding SOF/EOF short packet framing…
Part Number: DS90UB953A-Q1 hi Expert,
We need to cooperate with 1080p@120fps camera sensor and transmit CSI-2 signal through ti Serializer chip. The current problems are as follows:
1, DS90UB953A-Q1 The chip Up to 4 data lanes at 832 Mbps per each…
Part Number: DS90UB953A-Q1 Hi,
At the data sheet the filter is made of 3 FB (1.5K) and inductor parllel to resistor.
At the EVB there are 2 FB (47ohm and 330ohm) a resistor and the inductor parllel to resistor.
which one is the right one?
…