Part Number: DS90UB954-Q1 Other Parts Discussed in Thread: DS90UB933-Q1 , Hello TI team
We are currently working with the DS90UB933-Q1 (Serializer) and DS90UB954-Q1 (Deserializer) chipset. We need assistance with the specific register initialization…
Part Number: DS90UB954-Q1 Hi Team,
Can you help to provide the Errata sheets if any for the below parts?
DS90UB954TRGZRQ1
DS90UB960WRTDRQ1
DS90UB933TRTVRQ1
DS90UB9722TRURRQ1
TCAN1057AVDRBRQ1
TLIN1024ARGYRQ1
…
Thank you so much for your reply.
Hamzeh Jaradat said: such as data type, resolution and frame rate?
Image data from the imx412 camera RAW10 format Resolution 1920x1080 Frame 60 FPS
Hamzeh Jaradat said: i.e. how many Mbps/lane?
According to…
Hello,
essence Lee said: After applying the five register settings you suggested on the DS90UB954
Just to be clear, I have not suggested any thing. You asked me if it is possible to discard frames within our device and I provided the registers can…
Part Number: DS90UB954-Q1 Tool/software: The DS90UB953 is fed with two lanes at 780 Mbps. Can the DS90UB954 output over two lanes at 800Mbps (when using 25MHz clock)?
Is there additional overhead that would prevent a 800Mbps DS90UB954 lane output from…
Hi Yunseok,
From the UB953 Schematic: 1) On the pins VDDD, VDDDRV and VDDPLL the ferrite beads and 1uF capacitors are missing. Please refer to the datasheet figure 7-3. 2) On the MODE pin, for Synch mode, R66 must be open but it looks like a 10K is…
Part Number: DS90UB954-Q1 Hello,
My customer wants to know the rules for length-matching for FPD-Link differential traces. Could you answer that and provide any resources to help here?
Best,
Jason Maxwell
Part Number: DS90UB954-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 Hello TI Team,
Currently we are working on one project, where we are bringing up On Semi camera AR0544, connected using serializer and deserializer IC of TI.
Deserializer : DS90UB954…
Part Number: DS90UB954-Q1 Please provide COC and actual impedance mesurments data for MIPI CSI-2 DESERIALIZER, 6.4GBPS, DS90UB954TRGZRQ1, shipped to Gentex Corporation under PO# 3945191.
Part Number: DS90UB954-Q1 Other Parts Discussed in Thread: TS3DV642-Q1 Tool/software: Hi TI Team
We need a MIPI Switch and retimer for 2 DS90UB954-Q1 to SOC input
Does "TS3DV642-Q1" & "SNx5DPHY440SS" support DS90UB954-Q1 output singal?
SNx5DPHY440SS…