Part Number: DS90UB962-Q1 Hi team,
If LOCK is stable, can we check video status by reading 0x4E register?
Do you think there is any other register that can check video status? I recommend customer to check 0x73-0x76 register, but they told me that…
Part Number: DS90UB962-Q1 Tool/software: Hi Sir,
My customer want to design a receiver for truck application with 53ft cable length. Is DS90UB962 can be used at this application by using STP or Coaxial cable? Any TX device or cable spec. are required…
Part Number: DS90UB962-Q1 Tool/software: HI,we use DS90UB962-Q1 with 4 DS90UB933, it show the split camera picture as follows:
Do you have any idea what cause this ?
Thanks!
Part Number: DS90UB962-Q1 Tool/software: Hello Expert,
Could you please provide following information regarding reflow profile?
1.1) Upper limit of peak temperature under reflow heat resistance condition (Ex : 260° C).
1.2) High temperature…
Part Number: DS90UB962-Q1 Tool/software: Hello Expert,
Could you please answer following questions?
Could they change via diameter on thermal pad from recommended 0.2mm to 0.6mm?
I believe this via hold diameter have impact only for thermal…
Part Number: DS90UB962-Q1 Tool/software: Hi team,
The customer encountered a white line on the screen and needed to check whether the CSI-MIPI output of 962 had ECC or CRC problems; Do I have any fault registers to detect whether MIPI has ECC and CRC…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB935-Q1 Tool/software: Hello
We have encountered an ESD issue of our automatic parking system ECU, camera;
Issue 1 : The combined video screen is blurred while we discharging 6KV/8KV…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: ALP , USB2ANY Tool/software: Hi Team,
The customer uses DS90UB962(Serializer:DS90UB933), The following is the application schematic. How to set the internal registers of DS90UB962 using ALP…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: USB2ANY Tool/software: Hello TI experts:
we are facing some issues when using the UB962 and UB935.the source tickets can be found here.
e2e.ti.com/.../5623084
We are using the TDA4->UB962…
Part Number: DS90UB962-Q1 Tool/software: We are using the MAX96705 & MAX96706 components for video transmission.
We would appreciate your help in finding a component for converting Parallel data to MIPI (CSI-2) that can connect to the output of the…