Part Number: DS90UH926Q-Q1 Dear Team,
we have a question regarding serializers/deserializers for FPD-Link III.
So, we have application CPU that has HDMI or LVDS display output (we are looking for both). From other side we have small and low resolution…
Part Number: DS90UH926Q-Q1 Other Parts Discussed in Thread: DS90UH925Q-Q1 , Hi team,
My customer wants to know whether DS90UH925Q-Q1 has the same power-up sequence as DS90UH926Q-Q1 regarding VDDIO and VDD33.
I could't find power-up sequence description…
Part Number: DS90UH926Q-Q1
Hi team,
My customer thinks it is very hard to understand DS90UH926Q-Q1 datasheet Figure 6 Output Data Valid Times. The customer asks whether the figure (A) or (B) below is correct.
I think (A) is correct. Because there…
Part Number: DS90UH926Q-Q1 Hi,
I use 926connect with 927,and sometimes when I reboot the uh927, the panel lost display, and never recover unless I powerdown them and then power up. When the 926panel doesn't show the picture, I try to enable
pattern…
Part Number: DS90UH926Q-Q1 Other Parts Discussed in Thread: DS90UB927Q-Q1 , Hello Team,
When not using HDCP function, is it possible to connect DS90UB927Q-Q1(without HDCP) to DS90UH926Q-Q1(with HDCP, FPD-LinkIII->LVCMOS)?
Best regards, Kato
Part Number: DS90UH926Q-Q1 Hi,
Let me confirm about meaning of following spec.
Is above "noise frequency" included "ripple noise" of Vddio and Vdd33 ?
(Ex, if ripple noise is 40kHz and Vp-p is 80mV, there is no issue because Vp-p of noise is less…
Part Number: DS90UH926Q-Q1 Tool/software: Linux Hello guys:
I have used DS90UH926 in a digital dashboard, Now project start to pp but I have find about 7 units has display issues in 30 units, The issue is that there are several pix can not display…
Part Number: DS90UH926Q-Q1 Dear Team,
My customer use UH926 and UH927 on thier board design.
They would like to know which register of the uh927 is empty . And they can read/write any data into the registers.
Thank you.
Part Number: DS90UH926Q-Q1 Dear Team,
My customer would like to know how to initialize white balance?
Could you provide the sample code of white balance register value(Table 3) to them?
Thanks.
Part Number: DS90UH926Q-Q1 Dear Team,
As picture below:
When I write to SA ( VA(UH926)->SA(UH927) ), I hope the SA(UH927) will send a interrupt to SOC.
Do you have any suggestion?
I try to set the reg 0xc6 as 0x21 on UH927. But it doesn't work…