Part Number: DS90UH929-Q1 Hi, E2E members
Which pin is the power supply for internal PLL that makes FPD Link III data (Parallel:TMDS to Serial:FPD)?
PIN NO.17(VDDP11) is right?
Regards, Nao
Part Number: DS90UH929-Q1 Hi, E2E members Our system does not use CEC pin. How should it process the CEC pin? * Pull-up with a 27kΩ(+/-10%) resistor to 3.3V, right?
Regards, Nao
Part Number: DS90UH929-Q1 Hi, E2E member
I would like to know the reading sequence of EDID in the External local EDID (EEPROM) mode.
My understanding is here. 1. Connect HDMI Source cable to HDMI port in DS90UH929-EVM. 2. Turn on the RX_5V from HDMI Source…
Part Number: DS90UH929-Q1 Hi, E2E members
Can we connect External EEPROM (EDID) at SDA(14pin) and SCL(15pin)?
EVM user guide says, External EEPROM (EDID) connect DDC_SDA(44pin) and DDC_SCL(45pin).
Regards, Nao
Part Number: DS90UH929-Q1
Hi, E2E member
I confirmed power up seqence in ds90ub929-EVM. Original E2E QA say, Recommnd power up sequece is the follwing.
The recommended power up sequence is as follows: • VDD18 • VTERM (VDD33) • VDD11 • Wait…
Part Number: DS90UH929-Q1 Hi, E2E members
Our customer using VTRM by 3.3V.
Please tell me MAX supply current of VTRM.
The datasheet says, VTRM is 60mA(TYP).
We would like to know MAX spec of VTRM.
Regards,
Nao
Part Number: DS90UH929-Q1 Other Parts Discussed in Thread: ALP
Hi, E2E members
NOTE: This question is based on the following E2E. e2e.ti.com/.../735163
I have questions about FPD-Link output jitter spec. DS90UH929 datasheet says FPD-Link output jitter is…
Part Number: DS90UH929-Q1 Hi, E2E members Do you have test data IEC 61967-1, 2, 3 against IC or EVM? The customer ask it to me. They want to confirm the data for DS90UH929. If you test it, could you please provide the data? Regards, Nao