Part Number: DS90UR124 The DS90UR124 is used for communication, but there are some cases where there is no input signal.
When there is no signal in the input of RIN+ and RIN-, I thought that the output of the LOCK signal is L level, but it seems to be…
Part Number: DS90UR124 Hello E2E,
I know that this device transition to be power down mode when lost the LVDS input. Why doesn't TI list it in the datasheet?
Regards,
ACGUY
Part Number: DS90UR124 Other Parts Discussed in Thread: TFP401 Hi guys,
I want to make a design with the Raspberry Pi Compute module and 7" LCD display (which should be like 2-3 meters away from the PCB with the compute module).
I already bought…
ANSWERS
1) DS90UR124 and DS90C124 really support 18 bit color with HS/VS/DE
2) 3.3V LVCMOS levels
3) yes per DS90UR907 section 7.3.3 Video Control Signal Filter
4) yes
Part Number: DS90UR241 Other Parts Discussed in Thread: DS90UR124 , hi Sir
Due to insufficient FPGA IO, we currently want to use a set of outputs and inputs to drive more than two sets of DS90UR241/DS90UR124 respectively. The schematic diagram is as follows…
Part Number: DS90UR124-Q1 Other Parts Discussed in Thread: DS90UR241-Q1 Hello,
Isn't there IBIS model for DS90UR124-Q1?
There is one for DS90UR241-Q1 at TI website for everyone, but somehow not for UR124.
I if one for UR124 is available, please let…
Part Number: DS90UR124-Q1 Other Parts Discussed in Thread: TFP410 , DS90UR241-Q1 Hi Team,
I am trying to convert the RGB output of the DS90UR124-Q1 into a standardized output that I can put onto a screen and see my image. Something like VGA or HDMI. I…
Other Parts Discussed in Thread: DS90UR124 Hello
According to the data sheet of R124, it can support Data rte of 1.03Gbps.
I would like to know supporting range of Video as the below.
Please check the below table.
Thanks
RESOLUTION
FRAME
…
Hi Stefano,
The DS99R103 can only accept TCLK Input Jitter of 33 ps, so it is not recommended for SSC. Are you looking at only replacing the DS99R103 or replacing both devices?
Some SERDES pairs with similar functionality and SSC tolerance include
…
Hello
I would like to know whether the 124 & 241 can support BT.656 Video Signal format interface.
If anyonw who have experience for BT.656 interface for SerDes, let me know DeSeriel Configuration for Receiving BT.656 format.
Thanks and Best Rega…