Part Number: DS92LV010A Can you please provide the junction to case thermal resistance and the operating junction temperature range for part number DS92LV010ATM/NOPB?
Part Number: DS92LV010A Hello, My customer uses DS92LV010A as only driver mode. They would always like to disable receiver mode by pulling RE_ up to Vcc. Can they connect RE_ to Vcc directly? Or they have to put a resister, for example 10Kohms, between…
Part Number: DS92LV010A Hi sir,
I would like to ask about the terminal resistance of DS92LV010A differential line (DO + / DO -). Because it's differential, I think it should be 100ohm.
But why is 54 ohm used in the following applications in the datasheet…
Part Number: DS92LV010A Team,
My customer has the following questions:
Is there a weak pull up/down within the DS92LV010ATM device on the RE pin?
If pin 5 (RE) is left floating, what could be the behavior of the part or would there be any significant…
Part Number: DS92LV010A Other Parts Discussed in Thread: DS90LV012A , I am currently working on a layout for DS92LV010A and DS90LV012A. Is it better to lay it out as a “T” with 2 terminated LVDS branches or use a single much longer branch in a “C” configuration…
Part Number: DS92LV010A Hello all,
I am using at my board DS92LV010A - BUS LVDS 3.3/5V SINGLE TRANSCEVER,
I am searching for same component with lightning protection at the LVDS side.
My requirement for lightning is waveform 3 and 4 - level 3. …
Part Number: DS90LV027AH Other Parts Discussed in Thread: DS90LV028AQ-Q1 , SN65LVDS33-EP , DS90LV027AQ-Q1 , DS90LV011AQ-Q1 , DS90LV011AH , , DS92LV010A Hi,
There are 5 LVDS drivers that meet our requirements. DS90LV028AQ-Q1, DS90LV027AH, DS90LV027AQ…