Part Number: DS92LV0421 Other Parts Discussed in Thread: DS92LV0422 Dear team,
I still have some missing information regarding this package:
Sheets with thermal pad dimensions, footprint and stencil recommendations are missing In Mechanical Data…
Part Number: DS92LV0421 Hi Team,
I fould that the same signal meeting IC transmission format can transport well via DS92LV041(2), while DS90UB927(8)Q-Q1 can not transport the signal.
Could you please help by explaining the differences between DS92LV041…
Part Number: DS92LV0421 Other Parts Discussed in Thread: DS92LV0422 , Hi,
I am new to this concept of Serializing and deserializing the data.
So, please forgive me if my question is stupid.
I needed to know, if it is possible to interface a MIPI…
Hi Richard,
Yes, you can use the DS92LV0421 serializer with the DS92LV2422 deserializer. There are no compatibility or setup issues for this solution.
Regards,
I.K.
Part Number: DS92LV0421 Other Parts Discussed in Thread: DS92LV0422
Dear Sir/Madam,
I am using DS92LV0421 as serializer from LVDS input signal to CML output signal. Below is my setup for my measurement:
Here is my input waveform, look ok!…
Hi Brian,
Can you check all jumpers at default setting on both EVK boards? Can you send me a list of settings? What happens if you remove all input data and only provide a clock? Can you probe the input clock and see what the signal quality is.
…
Hi, Ryan-san
I looked into the IBIS model of DS92LV0421/2422.
DOUT+- and RIN+- are "NC (none connect)".
so, it meen that we can't confirm connection each other, right?
And then, we need to IBIS-AMI model, if confirm function of equalizer and de…
Other Parts Discussed in Thread: DS92LV0421 , DS92LV0422 I want to use the DS92LV0421 in BIST mode as test equipment (TE) to generate PRBS7 data to a Unit Under test (UUT). The data source and sink will be test equipment with the Unit Under Test (UUT…
Other Parts Discussed in Thread: DS92LV0422 , DS92LV0421 , DS90UB913Q-Q1 , DS90UB914Q-Q1 Hola,
We have a new application as below figure:
And we found device DS92LV0421 / DS92LV0422 which seems can support our application.
Just wants to confirm…
Other Parts Discussed in Thread: DS92LV0422 , DS92LV0421 , DS90UB940-Q1 , DS90UR910-Q1 Hello,
We need to serialize a MIPI interface and then de-serialize on the other end. The interface for the DS92LV0421 and DS92LV0422 look like they might do MIPI…