Part Number: DS92LV2412 Other Parts Discussed in Thread: DS92LV2411 Tool/software: Hi,
Our customer is currently mass-producing products using the DS92LV2412, and they have observed a lock loss issue particularly under cold temperature conditions in…
Part Number: DS92LV2412 Tool/software: Hi,
We are currently evaluating the DS92LV2412 device and would like to inquire about the following two points regarding the input specifications described in the datasheet:
Q1. Regarding the input eye diagram…
Hi Mario,
When devices in the BIST mode without applying any signal /frequency, do you see a high on PASS pin? Please follow 8.3.3 for testing BIST.
Is there a reason why you apply a signal (100-200Khz) on Din2 ?
Can you forward the system block…
Part Number: DS92LV2412 Hello E2E, They adopted DS92LV2412 for new product for scanner. It communication failed in test before pre-mass production. It occurs with a specific video(data) pattern. LOCK status pin to been low at the specific data pattern…
Hi Kawai-san,
I believe this was handled over email. Below is the answer given:
There are no concerns about 9MHz particularly. For the supply noise, normally we would prefer to have it below 20mV typically. With a 10uF cap and ferrite beads, normally…
Other Parts Discussed in Thread: DS92LV2412 , DS92LV2411 Hi all. I have one question about DS92LV2412. Please check Table 16 in the datasheet of DS92LV2411/DS92LV2412. There is discribed the PCB DAP size of DS92LV2412 is 7.2 *7.2 mm in Table 16. However…
Other Parts Discussed in Thread: DS92LV2412 , DS92LV2411 Hi all, I have two questions about this device. 1. about Deserializer There are only the wave standard values of VTH/VTL and VCM in datasheet, so i would like to know other standards value(for example…
Other Parts Discussed in Thread: DS92LV2412 , DS92LV2411 Hi all I have some questions about DS92LV2411,DS92LV2412. 【Serializer/Deserializer】 ・How long is the channel Link Ⅱdistance recomended between seializer and desirializer? I saw the datasheet P4…
Other Parts Discussed in Thread: DS92LV2412 Hi all, According to the datasheet of DS92LV2412, there is no power-up sequence between Vddn(1.8V) and Vddio(3.3V).
When the power up sequence is the following waveform, is there any problem?
Regards,…
Other Parts Discussed in Thread: DS92LV2412 Hello.
I am designing with DS92LV2412. The operation voltage is 1.8V. All of control & configratin pin is not pull-up or pull-down. configuration will setted by I2C. Question, need 3.3v pull-up to the serial…