Part Number: DS92LV2421 Other Parts Discussed in Thread: SN65LVCP204 , , DS92LV2422
Dear, TI
We are going to use the SN65LVCP204 crosspoint switch with the DS92LV2421 serializer.
SN65LVCP204 crosspoint switch was connected to via diff. 100 Ohm STP…
Part Number: DS92LV2421 Hello,
Our customer have a question about supply current.
In the specification of the IDDT1, does the VDD include all VDDx except for VDDIO?
Best Regards,
Naoki Aoyama
Part Number: SN65LVCP204 Other Parts Discussed in Thread: DS92LV2422 , DS92LV2421 , Hello
Can SN65LVCP204 be used between DS92LV2421 and DS92LV2422?
Check the below system are available
Regards.
Part Number: DS92LV2421 Other Parts Discussed in Thread: DS92LV3241 , DS32EL0421 Deas:
We are promoting the Solution to our LED WALL customer, and we have 2 issues about it:
1. From datasheet I can see below information and could it compute it? Since…
Part Number: DS92LV2421
Hi
We are searching the SerDes IC which supports YUV Input in catalog spec.
We are considering DS92LV2421, but it seems to support RGB only.
Do you have the serdes IC which can accept YUV data?
Or do you have an…
Part Number: DS92LV2421 Other Parts Discussed in Thread: DS92LV2422 Team,
I have a customer who is looking at using the DS92LV2421, but wanted to know the following:
"If I use this part in the system, can it work for an isolated system?
Consider…
Hello,
Actually the serial stream in addition to the 24-bit data also contains an embedded clock, video control signals, and the DC-balance information. Which comes to a total of 28bits, this means that the transmission rate is 28bits*25.175MHz =…
Part Number: DS92LV2421 Hi
I have questions about DS92LV2421/2422.
1. Does this device support YUV?
2. Is the control signal we can send data enable, HS, VS only?
3. I assume the following.
RGB/YUV -> Serializer -> Deserializer -> RGB…
Other Parts Discussed in Thread: DS92LV2421 Hello,
Our customer use the DS92LV2421/22.
The customer use these devices with VDDIO=3.3V and another VDDx=1.8V.
Is there any sequence of power up?
Best Regards,
Naoki Aoyama
Part Number: DS92LV2421 Other Parts Discussed in Thread: DS92LV2422 , , SN65LVDS93B , SN65LVDS93A Hi Sir
May we know if DS92LV242x can support 24 bit parallel to LVDS bridge IC (1280X720 60fps)?
or if you have other suggestion IC?
Bogey