Part Number: TMP432 Other Parts Discussed in Thread: DXP Hello,
In section 8.3.6 of the datasheet, it says the following:
When not using the remote sensor with the TMP43x, the DXP and DXN inputs must be connected together to prevent meaningless…
Part Number: TMP441 Other Parts Discussed in Thread: DXP Tool/software: Hi,
I am planning to use TMP441.
The SENSOR FAULT section states that the DXP/DXN pins should be connected when they are unused.
The link below states that DXP/DXN should…
Part Number: TMP423 Other Parts Discussed in Thread: DXP Tool/software: Hi Teams,
I’d like to confirm some questions regarding the signals on the DXP and DXN pins when VDD = 3.3V with PNP transistors:
As shown in the waveform below, the signals…
Part Number: DXP The installation of the DXP setup was successful without any error. When I open DXP DAC Exerciser Programmer, I'm getting a pop-up showing the VI is not executable. I have attached the pop-up. The DXP_Main.vi will freeze on searching…
Part Number: DAC81404EVM Other Parts Discussed in Thread: DXP Tool/software: Hi,
for evaluation I need to evaluate custom waveform from csv.
does this DAC81404evm work with DXP EVM GUI?
If not can you please recommend an alternative product including…
Part Number: TUSB212 Other Parts Discussed in Thread: DXP
Hi expert,
Referring to USB specfication Rev2.0 "7.1.1 USB Driver Characteristics", The USB port can withstand voltages from -1.0 to 4.6V.
In the other hand, Referring to TUSB212 datasheet…
Part Number: DXP Other Parts Discussed in Thread: DAC8814 , DAC8811 NI-VISA driver detected when connected to PC. When DXP is loaded, the device is getting listed in other devices as unknown device, it is not being recognized as USB devices.
Part Number: DAC8832EVM-PDK Other Parts Discussed in Thread: DXP , DAC8832 Hi,team
My c ustomer is using DXP Software to his DAC8832EVM-PDK .
he encounter error below.
Start the DXP software and set the status to USB connection waiting state.…
Part Number: TMP421 Other Parts Discussed in Thread: DXP For the TMP421, the data sheet states "If the remote channel is not utilized, DXP can be left open or tied to GND." However, nothing is stated about the DXN pin. How shall I connect the DXN pin…
Part Number: DXP Hi,
I recently downloaded and installed DXP DAC Exerciser program ( http://www.ti.com/tool/DXP ) and am immediately running into issues. The program installed without any issues, but when I start-up DXP, I am confronted with a File…