Part Number: TM4C1294KCPDT Hello.
I connect ADC pin to ground and got the measurement graphs of the measurement ADC values
I do same experiment with EKS-LM4F232:
Nosie about 10-15 counts. Why? For my LM3S5R31 i see ADC noise about 2-3…
I have LM4F232H5QD evaluation board. Whenever i run qs-logger application for collecting Accelerometer data and EK-LM4F232 board is connected to a host PC via the USB OTG cable then i get exact and fast Accelerometer data from the device. What i want…
Part Number: TM4C123GH6PM
Hello,
I am a student working on a senior design project utilizing the Tiva tm4c123gh6pm arm processor and am struggling to get the SPI slave interface to work correctly.
So far I have used an example from this form post…
I noticed the ORIGINAL_PROJECT_ROOT variable is still set to "C:/TI/TivaWare_C_Series-1.1/examples/boards/ek-lm4f232/usb_dev_msc/ccs".
What is this variable used for? Do I need to change it to the version 2 directory?
Hi,
An example in this location: Tiva-2.1.0.12573/examples/boards/dk-tm4c123g/qs-logger
Also boards/ek-lm4f232/qs-logger
Both with multiple channels.
Petrei
Hi Arden,
The Tivaware package for other Tiva kits has USB host examples. These below are what I found at Tivaware for my Tiva Connected Launchpad and EK-LM4F232.
usb_host_keyboard
usb_host_mouse
usb_host_msc
-kel
Hi Rashmi,
Are you using EK-LM4F232 kit? There is a blinky example program at the Tivaware. It has this #define include below.
#include "inc/lm4f232h5qd.h"
-kel
It has been a part of the TivaWare and StellarisWare releases since we introduces the DK-TM4C123G and EK-LM4F232 that preceded it.
C:\ti\TivaWare_C_Series-2.0\tools\logger