Part Number: ESD1LIN24-Q1 Tool/software: Hi We need your support to get IMDS data for all the products that we use in one of our design.
Currently, we are using the following TI products:
Mfg Part No.
Description
ESD1LIN24DYFRQ1
TVS DIODES AUTO…
Part Number: TLIN1039-Q1 Other Parts Discussed in Thread: ESD1LIN24-Q1 Tool/software: Hello experts,
As I am making a presentation for TLIN1039-Q1 to my customer tomorrow, I hope your immediate reply.
In the datasheet of TLIN1039-Q1, I found TLIN1039…
Part Number: ESD1LIN24-Q1 Other Parts Discussed in Thread: ESD761-Q1 , ESD761 Hi Sir,
May I know if the ESD1LIN24-Q1 can replace the Littelfuse SPHV15-01ETG-C or not?
If it can't, could you please advise the correct solution? Thanks!
Part Number: ESD1LIN24-Q1 Hi team,
As I know that ESD1LIN24-Q1 is bi-directional that just would like to double check can it be used in reverse?
Since the device pin config said pin1 is IO and pin2 is GND as below.
However competitor ESDLIN1524BJ show pin1…
Part Number: ESD1LIN24-Q1 Other Parts Discussed in Thread: ESD1LIN24 Hi Team,
Advantages of ESD1LIN24DYFRQ1 and general ESD electrostatic protection components,
Does LIN BUS have special specifications for ESD protection?
Part Number: ESD1LIN24-Q1 Hi team,
thanks for your support always!
I have a question here that my customer LIN bus system spec is:
Recommended voltage at pins DSI and DSI_O min to max is 4 to 20V, and Absolute Maximum Voltage Rating is 30Vmax.
Based on…
Part Number: TLIN1029A-Q1 Other Parts Discussed in Thread: ESD751-Q1 , ESD1LIN24-Q1 Hello team,
My customer is asking me about the below item. Can you tell me your opinion?
<Question>
- Is it OK to place a chip varistor between LIN(pin6) and GND?
…
Back to Interface Home Page
LIN Protection
Highlights:
LIN: Single ended data transfer interface
LIN clusters consist of 1 master and up to 16 slave nodes
Construction: One wire for data transfer + ground
Bidirectional configuration is needed to protect…
Hi,
For automotive, we don't have an automotive version of ESDS552 which is 12V in our portfolio currently. But for 24V, there are more options. There is ESD1LIN24-Q1 , ESD751-Q1 , and ESD761-Q1 which are all SOD323 or smaller and the main difference…
Part Number: TLIN1028-Q1 Other Parts Discussed in Thread: ESD1LIN24-Q1 Hello, I was given the following schematic, and I am reviewing it in parallel to this. Please let me know if it looks good. Thanks!