Part Number: ESD204 Other Parts Discussed in Thread: ESD122 , TPD4E02B04 Hi Sir
May I know TI have HDMI 2.1 ESD solution ? We have KVM customer request the solution ,if possible ,I would like to discuss this opportunity offline
Hugo
Part Number: ESD204 Hello team,
The clamping voltage waveform is shown at Fig.4 and 5 in the datasheet, but actually is the voltage measured on Connector side or System side?
Regards,
Jun
Part Number: ESD204 Other Parts Discussed in Thread: ESD224 , TPD4E05U06 Hi team,
(1) According to the datasheet, the recommended layout pattern is different between ESD204 and ESD224 as below. Could you explain the reason for the layout difference between…
Back to Interface Home Page
DisplayPort Protection
Highlights:
Data speeds up to 20Gbps
8 data lines, 20 total pins
3.3V, 500mA Input
Low capacitance required on data lines
Device
V RWM
Cap
(pF)
ESD(kV)
IEC61000-4-2
Contact
No. of Chan…
Part Number: ESDS314 Other Parts Discussed in Thread: ESDS304 , ESD204 Is ESDS314 able to protect 2.5Gbps EtherNET PHY? or what alternative solution? thanks,.
Regards
Brian
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation and Temperature
Top…
Hi John,
This will depend on what type of USB you're using and the voltage levels.
If you want a 4-ch device with higher IEC ESD ratings there are options such as ESD204 than can protect signals up to 3.6 V.
Our ESD and Surge Protection for USB Inte…
Other Parts Discussed in Thread: ESD204 Hello,
Does TI have recommendations for products to protect Ethernet lines from ESD transients on the cable side of the magnetics transformers? (pre-magnetics)
Thanks,
Dom
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…