Part Number: ESD2CANFD24-Q1 The ESD test requirements are as follows:
Post-ESD, the CAN waveform showed anomalies. Root-cause analysis reveals that the abnormal waveform tracks with the ESD protection diode.
The failure was attributed to a defective…
Part Number: ESD2CANFD24-Q1 Hi expert
Please can you offer the capacitance difference between the two branches for the CAN bus?
In the datasheet, I only find the line capacitance as below
Part Number: ESD2CANFD24-Q1 For lightning protection analysis, we need the graphical representation of Peak Pulse Power (watts) vs Pulse width (microseconds) graph which is not available in the datasheet.
Kindly provide it.
Part Number: ESD2CANFD24-Q1 Other Parts Discussed in Thread: STRIKE , ESD2CAN24-Q1 Hello team ,
I am trying to replace the part from nexperia PESD2CANFD with ESD2CANFD , all the features Vcl ,Vbr Vrw ,Ir and dimensions looks perfect ,only concern I…
Part Number: ESD2CANFD24-Q1
MAKER
PartName
Semiconductor process (Fab Process Fill in with numerical values )
Ex) 40nm,90nm etc.
Texas Instruments
ESD2CAN24DBZRQ1
Part Number: ESD2CANFD24-Q1 Other Parts Discussed in Thread: ESD601 , ESD2CAN36 Tool/software: Do TI have an bidirectional ESD protection device that can be used to protect a 100BASE-T1 interface but also withstand a STB fault of 52V.
Most devices I…
Part Number: ESD2CANFD24-Q1 Hi
We have a ESD requirement for 10GE Phy Interface.
Application = 2.5G/5G/10G Ethernet
Let me know if you could support us 4-line 10GE.
Regards
Prabhu
Part Number: ESD2CANFD24 Other Parts Discussed in Thread: ESD2CAN24 Hi,
In the datasheet of ESD2CANFD24, it says the working voltage is 24V. does that mean it can only work on the 24V CAN system? if there is a 5V/12V CAN system is it a proper device…