Part Number: ESDS312
Hi,
I see that ESDS312DBVR datasheet provides data for IEC-61000-4-5 Ipp as 25A for Absolute maximum rating. It is the same as Ipp value mentioned in Electrical characteristics. Usually in my experience, Absolute maximum values…
Part Number: ESDS312 Other Parts Discussed in Thread: TPD1E10B09
Tool/software:
Hi team,
I am looking for a bidirectional ESD diode with signal port protection. The maximum signal level is 7V and I want the clamp voltage to be less than 18V. Do…
Part Number: ESDS312 Hi team,
The datasheet states that it is an Easy flow-through routing package (ESDS312), so is it possible to connect IO1-NC and IO2-NC?
Best regards,
Part Number: ESDS312 Other Parts Discussed in Thread: ESD411 , TPD1E10B06 , THVD1500 Hi TI Support Team,
We are developing a custom Industrial Access Control System based on an embedded motherboard and are looking for your expert design/component recommendations…
Part Number: TIDA-010046 Hey,
on Page 23 of the design guide TIDA-010046 3V3 is at midpoint of the transformer and between 50 ohm resistors (first schematic for "non-PoE") and the ESD312DBVR is connected to datalines. Does it work correctly and are…
Part Number: ESDS312 Other Parts Discussed in Thread: ESDS314 , Hi Team,
what is the proper use of ESDS312 or ESDS314:
IEC 61000-4-5 Surge Class2 1kV 24A 42Ohm
-> When placing the ESDS31x between connector and ethernet magnetics?
Best Regards…
Part Number: ESDS312 Other Parts Discussed in Thread: TPD1E05U06 Hi sir,
In Page3 of ESDS312 mentions pins 1 nd 3 of the ESDS312 being available for straight through routing.
Could you further define straight through routing? Does that mean I can…
Part Number: ESDS312 Other Parts Discussed in Thread: ESDS302 Hi,
The recommended Input voltage range which is mentioned in ESDS312 data sheet is from 0V to 3.6V, so can ESDS312 be used as the surge and esd protection diodes for D+, D- and VBUS on USB…
Part Number: TMAG5115 Other Parts Discussed in Thread: ESDS312 , TMAG5213 Tool/software: Hello E2E Community,
We are planning to use the low-jitter TMAG5115 Sensor for our Speed sensing use case where we plan to measure 2 pulses per revolution to synchronize…
Part Number: TPD4E02B04-Q1 Other Parts Discussed in Thread: ESD321 , STRIKE , ESDS314 , ESDS312 Tool/software: Hi,
We use DP83822HFRHBR ethernet PHY and TPD4E02B04QDQARQ1 TVS in our board.
In datasheet, PHY's TD and RD pins have absolute maximum voltage…