Part Number: ESDS452-Q1 Hello Team ,
Please confirm when use ESDS452-Q1 for single channel application , whether we can keep the unused channel as open/left connected .
ESDS452-Q1 used for sinlge channel application to maintain BOM part.
Part Number: ESDS452-Q1 Other Parts Discussed in Thread: ESDS552 , ADS1261 , ESDS452 Tool/software: This TVS diode array is drawn as two separate bidirectional TVS diodes in the datasheet:
The working voltage is +-5.5v, so I'd expect IO channel 1…
Part Number: TPS25762-Q1 Other Parts Discussed in Thread: ESD2CAN24-Q1 , , TUSB1021-Q1 , ESD1LIN24-Q1 , TPD4S201-Q1 , ESDS452-Q1 We kindly request a schematic review for our USB 3.1 Gen 2 Type-C design which is used for the IVI application
The ESDS452-Q1 is bidirectional and has a clamping voltage of 8V in a SOT23-3 Package. Additional testing would be required to see if the diode could withstand the duration of the event.
The Protection Devices team does not have SIDAC. I will reassign…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…
Hi Knud,
Glad the ESD2CAN24-Q1 is working with the setup! Do you happen to still have the ESDS452 units that were failing? I would be interested to may be do a failure analysis on the part to see if there was any damage to the part.
Best,
McKen…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…