Part Number: EVMK2EX Tool/software: Dear Sir/Ma'am,
We want to provide IPMI, BMC feature in our design which is based on Altera/Intel Agilex 7 FPGA. For IPMI, BMC we want to use TI micro controller which is widely used by people for IPMI, BMC. Please…
Part Number: EVMK2EX Hi,
We are working on the K2E board NetCP Application with yocto version krogoth 2.1 and kernel version 4.4.32.
Here I am facing an issue in transferring packets using ethernet port0 or eth0, I am using SendPacket() and ReceivePacket…
Part Number: EVMK2EX Hi, all
Now our team use EVMK2E board normally with default flash setting (U-boot on NOR Flash, others (file system, kernel...) on NAND Flash),
We know EVMK2E support SATA driver and want to put others (file system, kernel...…
Part Number: EVMK2EX Hello.
I tried to install ubi file system on EVMK2EX using uboot commands.
I changed ubi_name as "arago-base-tisdk-image-k2e-evm.ubi".
The "arago-base-tisdk-image-k2e-evm.ubi" file is from in ti-processor-sdk-linux-k2e-evm…
Part Number: EVMK2EX Other Parts Discussed in Thread: 66AK2E05 , UCD9090 Hi, all
I want to monitor temperature of EVMK2E board.
On EVMK2E board, do it have internal temperature sensor or function to detect board' s temperature.
Does 66AK2E05 chip…
Part Number: EVMK2EX Hi team,
My customer has been designing AM62 by reference to EVM2KX. Could you please tell me the impedance control value of Y2_P, Y2_N, Y3_P and Y3_N?
Best regards,
Shunsuke Yamamoto
Part Number: EVMK2EX Hi,
I change the DDR3 so-dimm to a 4GB NON-ECC one.
Set ECCCTL to 0 (ECC disabled)
After Boot into POST. Read DRAM Address 0x80000000 cause system hang
Use any size of DDR3 w/o ECC, system still hang.
The same configuration…
Part Number: EVMK2EX Hi,
Recently, I'm using EVMK2EX and find out application running time is slow.
I know that EVMK2H have same ARM cores with EVMK2EX. So I put the same application to EVMK2H to run and see that was faster.
I check the BogoMIPS…
Part Number: EVMK2EX Other Parts Discussed in Thread: PMP , DA8XX Cold start of the EVMK2E with a SATA drive connected produces the following error during the boot processes.
[16.858571] dwc3 2690000.dwc3: Failed to get clk 'ref': -2
The /dev/sda…