Part Number: EVMK2EX Other Parts Discussed in Thread: 66AK2E05 , UCD9090 Hi, all
I want to monitor temperature of EVMK2E board.
On EVMK2E board, do it have internal temperature sensor or function to detect board' s temperature.
Does 66AK2E05…
Mike,
You are always welcome to modify the scripts of 10.4 CCS and make use of it.
As the EVM and SDK were tested with the recommended CCS 9.3, I am insisting to use them.
Otherwise, feel free, to use 10.4. I
f without any issues, CCS 10.4, works for…
Part Number: EVMK2EX Hi Experts,
Good day.
I would like to confirm if the development board device for Keystone 2 TI SoC with part number - EVMK2EX , come with its own power supply upon order? Its " What's included " link doesn't mentioned it, while…
Part Number: EVMK2EX Hello Team,
My customer received the EVM k2e board and used the wrong power brick (18V) instead of the 12V. Can this be easily repaired? They can see it has a zener on the input with a breakdown voltage of 13.3V. The 12V input is shorted…
Part Number: EVMK2EX Hi, all
Our team has bought the TI EVMK2E board for study. I have two question about TI EVMK2E:
(1)Form the speed register, EVMK2E support 1.5GHz.Is it true or have other limitation? From introduce of EVMK2H CPU, the high frequency…
Part Number: EVMK2EX Hi,
I add some code in C:\ti\pdk_k2e_4_0_16\packages\ti\platform\evmk2e\platform_lib\src\evmc66x_uart.c
I'd like to rebuild the platform_lib
But after "gmake pdk under C:\ti\processor_sdk_rtos_k2e_6_03_00_106" or
"gmake…
Part Number: EVMK2EX Hi,
I am reading the AM5K2E0x Multicore ARM KeyStone II System-on-Chip (SoC) data sheet
6.1 Memory Map SummaryAM5K2E0x shows that DDR3 data physical address mapped on 08 0000 0000 ~ 09 FFFF FFFF
I don't understand how to access 40…
Dear Customer,
Our sincere apologies for late reply. Thanks for your patience.
Please go the product folder of EVMK2EX and click on "order and start development" tab.
EVMK2EX Development kit | TI.com Find all the necessary Software packages needed…