Part Number: EVMK2EX Hi,
Recently, I'm using EVMK2EX and find out application running time is slow.
I know that EVMK2H have same ARM cores with EVMK2EX. So I put the same application to EVMK2H to run and see that was faster.
I check the BogoMIPS on…
Sorry copied the wrong log files.
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94-gbe5389fd85 (psteinhofer@spica) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel…
Dear Customer,
Sorry for the late reply.
yes, it is possible to retrieve the old u-boot.
u-boot comes along with the MCSDK SW package.
Go to the TI MCSDK download link, where you downloaded the package, scroll down to the end of the TI page and find the…
Part Number: EVMK2EX Hi,
I see that the latest PROCESSOR-SDK-LINUX-K2E is 06.03.00.106 released 04202020. This version is based on linux-4.19.94.
I am looking for older version that may be closer to linux-3.10
Kindly let me know how I can find that.
Thank…
Part Number: EVMK2EX Hello!
I believe the README document in the SDK for loading the u-boot SPI image into flash has an error.
It specifies the wrong variable to use to set the copy-from address for the burn operation. If you follow the README document…
Part Number: EVMK2EX Tool/software: TI C/C++ Compiler Hello,
I am trying to run the image processing demo on evmk2e board, but the arm kernel can't boot. when powered on, it printed serials of numbers and characters. i gave any commands, it had no…
Dear Customer,
Apologies for the delayed response and thanks for your patience.
Processor SDK is the next version of MCSDK.
You can go ahead and start with Processor SDK given under the product folder of EVMK2EX
PROCESSOR-SDK-LINUX-K2E
Regards
Shank…
Part Number: EVMK2EX Hello, Customer failed to run the OpenCL image processing demo on EVMK2E. When running ./runtests according to the processor SDK developer guide, the log is below and the opencv_test_log.out file is empty.
software-dl.ti.com/.../Foundational_Components_OpenCV…
Part Number: EVMK2EX Other Parts Discussed in Thread: 66AK2E05 Hello,
Just as the title says, does the EVMK2E with 66ak2e05 support the image processing demo. Is there any other demo which use IPC between ARM and DSP on EVMK2E.
Thanks,
Sua…
Part Number: EVMK2EX HI,
Does the stock TISDK for EVMK2EX support controlling GPIO pins on the EVM ?
If so, how do we exercise them, any linux commands ? is this a kernel module or an app ?
Any procedure to load/initialize/invoke to use those pins ? …