Hi Hank,
Halcogen includes FEE driver (TI FEE Driver User Guide is under HALCoGen Docs folder).
Flash API driver you have to download from TI's web site: www.ti.com/.../F021FLASHAPI .
Best regards,
Miro
Hi Huseyin Alperen,
In general Hercules F021 Flash API library will be used for erase, program and verify of flash in Hercules controller including TMS570LS3137 controller.
F021FLASHAPI Driver or library | TI.com
And the source code for this library…
Hi PGC
The Errata document is outdated, I will take necessary action to get this updated.
Meanwhile the latest Errata ( Known Issues ) in the F021 Flash API wiki page.
http://processors.wiki.ti.com/index.php/F021FlashApi
Hello,
Please download flash API library from:
www.ti.com/.../F021FLASHAPI
Please use uniflash or CCS8.x to program code to flash:
www.ti.com/.../uniflash
The reference manual of flash API is located in docs folder of the installation directory…
Also know that the F021 Flash API is delivered/installed with teh HalCoGen tool as well as available for stand alone download on the F021 Flash API product page located at this link: www.ti.com/.../F021FLASHAPI
Hello Needhu,
1. The F021 Flash Application Programming Interface (API) provides a software library of functions to program, erase, and verify F021 on-chip Flash memory.
The library is located at : www.ti.com/.../F021FLASHAPI
2. The reference manual…
Part Number: TMS570LC4357 Other Parts Discussed in Thread: HALCOGEN , TMS570LS3137 Hi Team,
I am using the Flash library F021 from https://www.ti.com/tool/HERCULES-F021FLASHAPI for TMS570LC4357 HDK.
During initialization of Flash library the function…
Hi Tammy,
To perform any of the following In-System flash operations, Erase, Program and Verify you need to get and use the F021 Flash API: www.ti.com/.../f021flashapi
Best Regards,
Christian
Hi, Sorry for the delay in my response.
These errors are due to not generating basic code from HALCoGen,
If you generate the code from HALCoGen then this directives will be defined in the below file
I created a example code for you, so please…
Hi Peter,
Yes, the F021 flash APIs can be used to erase/program the flash. The user guide is located in the installation folder of the Flash Library:
This is the link to download the Flash API:
https://www.ti.com/tool/HERCULES-F021FLASHAPI