Juvf,
1) Files that did not change from earlier versions were left as is so that users can easily identify the changes made.
2) When I set your search string on the ti.com, the first webpage that showed up is http://www.ti.com/tool/f021flashapi .…
Hi Rakesh,
Rakesh Dara said: I am using TMS320F28335 controller in this i want to perform single location FLASH erase is it possible or not
You can use Flash API to perform this operation. For more info refer and download from this link:
http:/…
Hi,
thank you for the answer.
So being the overhead 24bytes, I need to set my blocks at 4120 to write 4096 byted on them. That's Ok.
I don't understand the virtual sectors. How big they are? Where can i set the size?
Are my blocks too big? The…
Hi John,
I'm not really sure what issue you are wanting addressed. However, the F021 Flash API is a library of functions used in developing applications that program the flash in the Hercules devices. It is developed separately from CCS and is a stand…
Hi John,
Could you please provide the software package for FO21 Flash API Version 1.50.0.
We had tried by downloading with this link http://www.ti.com/tool/HERCULES-F021FLASHAPI . So, we got the following errors.
Regards,
Anand Kumar N S
Hi Furkan,
1. HDK supports more features such as EMIF SRAM, connectors for RTP/DMM, MIPI connector for ETM, and SUB transceivers and connectors, etc. But I think the launchpad is good enough for evaluating the device.
2. TI code composer studio is…
Chuck,
BTW I have solved the problem ... I installed the F021 API (downloaded spnc033.zip from http://www.ti.com/tool/f021flashapi) and then added the location of the library and include files to the project. I was able to then build the project and…
I was wondering if the driverlib flash.c and flash.h are going to be update to allow for reprogramming of the flash.
I know that this http://www.ti.com/tool/f021flashapi exist but in my situation I need full .c/.h source access.
Other Parts Discussed in Thread: F021FLASHAPI , HALCOGEN , TMS570LS3137 When using the F021 Flash API 2.01.00 I got the following error for different files:
error #16004-D: file "../vendor/F021FlashAPI/F021_API_CortexR4_BE.lib<Read.WdService.obj>" has…