Part Number: AM3354 Dear Sir,
When transplanting wm8960 sound card on AM335x there's some trouble. Urgently need the master's advice to help me to solve the problem. Question as below: Now the situation is that when playing audio files through aplay…
Hi Biser,
Yes. External pullup's are connected on the I2C lines.
W/WO external pullup's on the WAKE and INT lines also tested but the problem still present.
Using Oscilloscope probed the I2C lines i am not seeing I2C clock generated from processor…
Hi Prabhakar , Thanks for you valuable support. As per your suggestion changed RTC driver & device tree then updated new images (kernel and device tree) in board. We found that during boot hw clock not working and when execute "hwclock" in kernel that…
That is on the beaglebone black. first is with weston issue and the other one is without the issue
U-Boot SPL 2016.05-g2f757e5b2c (Oct 03 2016 - 17:53:44)
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args…
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: DP83848C , AM3352 , TPS65910 Tool/software: Linux Hi,
I am using TI Sitara PSP having Linux version v4.4.41. I am porting Linux on my custom board. I ported linux v3.2 successfully on…
hi, i am using ti-processor-sdk-linux-am335x-evm-03.00.00.04 linux-4.4.12+gitAUTOINC+3639bea54a-g3639bea54a
/////////////////Boot Log////////////////////
Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup…
Hi Christian,
We tested v4.4 kernel with ubifs and subpage test on AM335x EVM and both pass. We are not passing any arguments to ubiformat and ubiattach to override the default subpage size.
ubifs test pass log:
Starting kernel ...
[ 0.000000]…