Hi,all.
I want to use Flash tool to write xloader,uboot,kernel by usb.
But When I use the software, I find x-loaderand uboot was placed in one dropbox.In that dropbox,there were two items:
X-LOADER/U-Boot
Kernel
.but there are three images:…
Other Parts Discussed in Thread: FLASHTOOL It does not seem that the CCS Flashtool (nand_flash_writer_AM335x.out and/or NAND_Flashing_Tool.out) for the AM335X uses the files in the nandlib folder that are part of StarterWare. Is that true or am I missing…
Other Parts Discussed in Thread: DRA746 , UNIFLASH Hi All,
1. I want to know the debugger that can be used for Jacinto 6 DRA746.
Here ,http://www.ti.com/product/DRA746/toolssoftware XDS100 and XDS200 are mentioned but if I check
http://processors…
Hi micheal
Me too facing the same problem. our mass production plan is >8K . So CCS and JTAG method is not satisfy us. we prefer standalone single click NAND flashing tool for AM335X family from TI engineers.
Kindly release the Flash tool how soon…
Other Parts Discussed in Thread: FLASHTOOL Hello,
I am trying to use the FlashTool V1.5.1.0 for accessing a custom DM37 based CPU Board. Following the porting guide I need some help in customising the FlashTool configuration files. Specifically, I…
Other Parts Discussed in Thread: FLASHTOOL Hi,
I got an old OMAP3530Evm board, I just want to erase the buildin WinCE, to write the uboot and linux;
but the current flashtool does't have the option for that board with 256M Ram/256M Nand. heard…
Other Parts Discussed in Thread: FLASHTOOL , AM3505 I'm trying to use UART3 with FlashTool V1.6 on my custom AM35XX hardware. Since I am using Micron NAND Flash and DDR2 SDRAM I am using the default config file.
When I turn on my custom hardware FlashTool…
Part Number: AM3517 Other Parts Discussed in Thread: FLASHTOOL , UNIFLASH We're seeing ECC errors using TI's 2nd loader (dnld_startup_omap3_gp_2g.2nd) + NAND flash driver (nand_onfi_16bit_8bit.bin) to program NAND with BCH8 ECC. (I believe these binaries…
Part Number: TMS320F28374D Other Parts Discussed in Thread: CONTROLSUITE , FLASHTOOL Hello,
We need to update the TMS320F28374D device's fw inside a Linux (Ubuntu) environment.
We have already succeeded to do that in a Windows environment with the…
Part Number: AM3505 Other Parts Discussed in Thread: FLASHTOOL Hi,
Customer download firmware to AM3505 on USB during boot.There is a USB driver in WIN-XP for connect to AM3505, but it can not used in WIN7. The USB driver is released in 2006, we doubt…