Part Number: FLAT-CLAMP-TVS-EVM Hi
Please can you provide the CE/EU Declaration of Conformity for FLAT-CLAMP-TVS-EVM?
I could not find this on T.I website.
Thank you in advance
Part Number: BQ79718B-Q1 Dear TI Support Team,
We're designing a BMS using BQ79718 for an 18S battery pack and have encountered a TVS selection issue.
System Parameters:
18S configuration, 4.25V max/cell → 76.5V pack maximum
BQ79718 absolute…
Part Number: FLAT-CLAMP-TVS-EVM Hello experts,
I have question about TVS series IC.
TVS series have some IN pin (Surge Protected Channel).
But layout example in datasheet shows that this IC protects one signal line. EVM schematic also show same…
Part Number: TVS3301 Other Parts Discussed in Thread: TVS2201 , Tool/software: I want a flat clamp diode rated around 40-45V. I'm able to find is maximum rating of 33V (TVS3301). I'd also like to know if putting 2 diode rated for 22V (TVS2201) make it…
Part Number: TVS3300 Other Parts Discussed in Thread: MCT8329A , TVS1800 Tool/software: Hello,
I need the device with flat clamp at 60V, something like TVS3300 but for 60V and about 30A.
I can have a margin of 58-62V.
Can you suggest simplest possible…
Part Number: DRV8889-Q1 Other Parts Discussed in Thread: TVS2201 , TVS3301 , , DRV8452 , DRV8461 , DRV8462
Tool/software:
I want a flat clamp diode rated around 40-45V. I'm able to find is maximum rating of 33V (TVS3301). I'd also like to know if…
Part Number: TPS2660 Tool/software: Hi Team,
I have a question about Vin TVS selection,
We know the 70V is TPS2660 abs max voltage rating which device can tolerate for short pulse like 10 mS (datasheet value).
But my question is, most of the TVS…
Part Number: PMP10350 Hi Team,
We tested the PMP10350 evaluation board with a 265 VAC input and a 12 V / 1 A output. During testing, we measured the voltage across the MOSFET drain-to-source pins using extended wires from the evaluation board. The PMP10350…
Part Number: TPS25751EVM Other Parts Discussed in Thread: TPD4S201
Hi team,
My understanding is that TPD4S201 is connected on this EVM mainly for ESD protection and short‑circuit protection of the USB Type‑C CC pins.
However, the CC pins are…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1HC30-Q1 , TPS272C45 Hello,
I am using a high-side driver (TPS1HC100-Q1) to drive an inductive load.
The single pulse turn-off energy for this high side driver is 35mJ.
But, energy…