Part Number: FMC-ADC-ADAPTER Other Parts Discussed in Thread: AFE5818 We have AFE5818 EVM board. It has the board to board ADC LVDS output connector. And also I have the Xilinx KC705 EVM. It has FMC connector. I found FMC-ADC Adapter in TI store. Could…
Part Number: ADC12DJ3200EVM Other Parts Discussed in Thread: ADC12DJ3200 , , ADC12DL3200 Dear Sirs,
I will buy the ADC12DJ3200 EVM. In my design, I'll connect this EVB board to a Carrier board with FMC connector.
I've read that together the ADC12DJ3200EVM…
Hi tt,
Here's the link for FMC-ADC-Adapter passive interconnect board enables the output of TI’s High Speed ADCs LVDS output to be directly connected to a standard FMC
You can use this to connect ADS5560EVM to FPGA board's FMC connector.
Regrads…
Other Parts Discussed in Thread: ADS5400EVM , FMC-ADC-ADAPTER , ADS5400 Hi,
The pin names on the J2 of FMC-ADC-ADAPTER are exactly opposite to the pin names on the J4 of ADS5400EVM ,i.e.,IO_2 N ===>DA_11 P , IO_2 P ====>DA_11 N ,while the connection…
Part Number: ADS5400EVM Greetings
I am having trouble routing the CLKOUT signal from the ADC board to the ZC706 board and using it as a clock.
The pins I am interested are shown here on the evm,
Then routed to the FMC ADC adapter board…
Part Number: ADC12DJ3200EVM Other Parts Discussed in Thread: ADC12DJ3200 , TIDA-01024 Hi,
I am Tong Duan, from the University of Alberta. We want to connect two Xilinx VCU128 FPGA boards together using the FMC+ connectors. But now we only have a FMC…
Part Number: ADS8598H hello i have made parallel interface on fmc to stm32h745hix6
i want to read the data but facing issue while reading
please can anyone help me one-on-one
Part Number: ADS5282
I am working on a project that involves SP605 xilinx eval board and an ADS54RF63EVM ADC eval module (along with the ADC to FMC passive adapter board). I'd like to capture ADC output and send it out of the gigabit ethernet interface…