Hi Hareesh
Question 1: It looks the programming tool on JTAG from TI (FTLF240X & SPRC074) are both obsolete. The only tool I can find is C2Prg ( www.codeskin.com/programmer) +XDS emulator. Any other JTAG programming tool is available? It is better this…
Kailun Liu said: 1. Does the IC have to use CCS3.1-CCS3.3 to program?
You can indeed use CCSv3.3 to program. However, note that (unlike new Eclipse-based versions of CCS like v12.x), CCSv3.3 is not free. Alternately, you can use DOS command line utilities…
Jorge,
As you may be aware, this is a 20+ year-old device. The entire toolchain for these devices is now obsolete and there is very limited support for these devices (support now is only through e2e). There are two options for you to program this device…
AnBer,
The flash support for the LF240xA family can be found here: https://www.ti.com/tool/FTLF240X#ccspi
(expand the "view more") to see the list.
The two I'm most familiar with is the SDFlash tool, this is standalone GUI that will work with…
Arunkumar,
Please take a look at these 2 threads:
https://e2e.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/925143/tms320lf2406a-programm-the-tms320lf2406a/3418094#3418094
https://www.ti.com/tool/FTLF240X#supportandcommunity
Vinoth,
There are primarily two ways to program the flash (3, if you include SPI method, but it is a bit more involved), JTAG & Serial port.
If you have a working copy of CCSv3.3, you could program via the Flash plugin (i.e. the tool built into CCS…
Saravanan,
No, it is not possible to program flash using parallel port using CCS3.3v
These are some of flash programming options for F2407A. If you are looking to program F2407A in production environment, there are 3rd party which support that. Below…
Other Parts Discussed in Thread: FTLF240X HI
I got a board to reverse engineer.This board is located on the TMS320F240.
HOW I flash-eeprom reading this device .
Rory,
I have always used XDS510PP emulator to work on F240 devices. So, I would suggest the same. Regarding the error message about unrecognized processor code, I believe you are trying to invoke flash plugin (On chip flash programmer). In F240, CCS doesn…