8787.AWR1xx_Radar_Interface_Control.pdf Hello,
The information about the TX power backoff code can be found on Pg 72 of the AWR1xx_Radar_Interface control document found in the mmWave DFP.
TX0_POWER_ BACKOFF
1byte
TX0 output power back off
1LSB…
Tool/software: TI C/C++ Compiler Hello all,
We are facing linking errors while running makefile using cl2000 compiler.I am not using CCS tool or resursive make environment for building the source code.I am using a non-resursive standalone makefile for…
Other Parts Discussed in Thread: AWR1843
We recently ran into an issue with our AWR1843 hardware version that uses the TI ODS antenna pattern, see below. We’re running a modified version of the MRR demo that TI provided. We had to modify the angle estimation…
The signals i'll reply for you within tomorrow but I don't understand what do you mean "set GPIO61 to a GPIO but then set it back to the hardware SPI CS" Which line It's set back to GPIO? I
I use a original code but it set SPI-C so I need to change…
Hi Tim,
To decode an error, follow the process below:
Each error is a 32 bit value. bits 31:16 are the error type. If you take your value and right shift 16, you will get this value. For example, the first error you show is -203685722. Right shift…
spru714 datasheet.pdf TI RefDesign guideline.pdf DC-PLC Refernce Design.pdf Hi,
I am working on PLC, give me the solution for following requirements for PLC:
Carrier modulation: BPSK
Carrier Frequency:132KHz
Power Line Voltage:220VDC
Data Rate…
AWR1xx_Radar_Interface_Control.pdf Hello,
In the radar Studio documentation, there is an ICD document, I will attach it this time. Under the Initial Self test, and the Repetitive testing there is a bit mask for each test. Once you know which bit field…
Hi Koichiro-San,
I think you might be referring to a different version of the ICD which might not be completely applicable for AWR1843. You can use the below version.
5758.mmWave-Radar-Interface-Control.pdf
Koichiro Tashiro said: Q1) According…
Hi Manikandan,
It is present in the below datasheet :
J784S4_Datasheet.pdf
Section having the timing data(HS400 mode) which is basically HS200 DDR.
Regards
Gokul