Hello.
This is because the firmware has set a limit of 512 chirp loops within a single chirp cycle as this is the maximum that the hardware can support. You can refer to the ICD for more on the various valid ranges for different chirp parameters.
…
Parthipan Siva said: 1) is the valid values of <txOutPower> for IWR6843 same as the AWR1642? Above forum post stated valid values are [0,1,2,3,4,5,6,12,18,24,30]
The ICD says that it's supported in steps of 3 dB.
Parthipan Siva said: 2) What was…
Part Number: TDA4AH-Q1 Other Parts Discussed in Thread: TDA4VH Tool/software: New hardware design for
TDA4AH88TGAALYRQ1
TDA4VH, TDA4AH, TDA4VP, TDA4AP series
I am starting a new design for this Ti SOC.
I have a few questions.
For the DDR4…
The TI compiler help available in Code Composer Studio can be updated to contain the older manuals. The process is similar to updating the compiler, as described in this video , but instead of expanding the entry for TI Compiler Updates , you expand the…
No it doesn't. The example is totally different. Sorry George but you're wrong.
In a 32-bit 2s representation, a "signed long" number N is within the range: [-2 31 , 2 31 - 1]. This means its minimum value is -2 31 = -2147483648.
Please see below…
Hi Adam
attached the only two TMS320C28x Optimizing C/C++ Compiler User's Guides (v6.2 and v6.2.4) published before v6.4.
spru514f.pdf
spru514g.pdf
Regards, Bernd
Hi Alix
I was following the below pdf file to dump The excel file is compared result, I dump the five-time, the last one I restart the TAS5754M, and find the very different with before, It was same.xml to dump. Could your explanation register page.45…
Other Parts Discussed in Thread: TMDSHVMTRINSPIN , MOTORWARE , TMDSCNCD28035 , CONTROLSUITE Hello,
Is there any trouble i f I only want to DEBUG some program in CCS V6 without connecting the PC to TMDSHVMTRINSPIN?
If that is possible, which configuration…
Hi Gerd,
I discussed this issue with some of the C2000 experts. They were able to point me to the correct document for C2000:
/cfs-file/__key/communityserver-discussions-components-files/171/SPRU151A.pdf
However your issue of why you are unable…