Other Parts Discussed in Thread: DRV8307EVM Hi,
My customer tries to operate motor with DRV8307EVM. They use the hall element. it is "HW-105W". VM=24V.
At this case, What are we select at JP3 and JP4? I think think that we select the following. Is…
Other Parts Discussed in Thread: MOTORWARE , DRV8301 hi I use the DRV8301HC -C2 -KIT , I Have been testing PROGRAM (lab ) in motorWare .now I want to turn my motor PMSM with Hall effect sensor . what program should be used to control suite, (it is sensord…
Part Number: DRV10983 Dear TI Support Team,
We are using the DRV10983 motor driver for our BLDC motor application.
Initially, we tested our motor using the DRV10983 EVM development board . The motor runs smoothly and continuously at the required speed…
Hi,
There is no COM port for DRV10970, can you verify HALL connections?
Verify HALL angle placement 0 or 30 degree and HALL biasing.
Please refer to the EVM user guide DRV10970 EVM User's Guide
Thanks and Best regards
Venkatadri S
Hi Suren Porwar
when I quckily start the Altia demo
it log is
May 30 05:49:21 am62pxx-evm HyperCluster[249]: Altia code gen message: drmOpen() failed. May 30 05:49:21 am62pxx-evm HyperCluster[249]: driver_wm_error 100 May 30 05:49:21 am62pxx-evm…
Ryder,
We have a ref design that uses the LDC1314 inductive sensor for angle estimation: https://www.ti.com/tool/TIDA-00508 . It is oriented towards 1deg absolute accuracy and 0.1deg resolution, but it could serve as useful starting point. A higher…
Part Number: SK-AM62P-LP Other Parts Discussed in Thread: AM62P , AM62P5 Hi, I am using latest sdk in my evm (tisdk-default-image-am62pxx-evm-11.01.16.13.rootfs.wic.xz )
I Have connected display using HDMI connector and I am able to see the ti-apps…
Hi Rajesh,
Thank you for the quick reply.
The EVM's datasheet does not specify it anywhere, so I wonder, would your official EVM+GUI setup generate any signal output without Hall sensors attached? The chip itself can drive sensorless FOC after all…
Part Number: DRV8334EVM Other Parts Discussed in Thread: DRV8334 Hello TI Support Team,
We are using the DRV8334 EVM to drive a 24 V Ametek BLDC blower motor with 6-step trapezoidal commutation , controlled entirely via MCU-generated P WM signals. No…
Part Number: AM625 Device/SoC: AM6254ATCGGAALW Use case: HMI (graphics UI), without active cooling Form factor: Custom SMARC-size SoM + carrier (EVM-SK2-like schematic, same PMIC & active parts) Operating point: CPU @ 1 GHz (extended industrial range…