Part Number: J6EVM5777 Other Parts Discussed in Thread: DRA742 , PMP , DRA752 , TVP5158 , CSD
Hi,
I am trying to boot J6EVM5777 with Android Oreo following the instructions in the Release notes using pre-built binaries
However the Services keep…
Part Number: PROCESSOR-SDK-AM62X
Hi,
We developed an app and run on the am62x evm.
I found a problem that there is almost 1 second delay when switch activity(Image).
And the system log always display below log when the activity switched.
How…
Hi Hong, Here is SDK8.4 full log. Below line seems the error happens. [ 2.084076] mmc0: mmc_select_hs200 failed, error -110 SDK84_log.txt The customer does not keep SDK8.6 log, but the similar error was observed. Thanks and regards, Koichiro Tashiro
Hi,
Attached are the Boosterpack Pinout and MSP430F5529LP User guide. Please see Figures 40 & 41 in User Guide for Launchpad Pinouts. The unused lines (GPIOs) on the P2 & P3 of the BOOSTXL-CC1120-90 can be used for your Keypad.
If you change the Pins…
Part Number: DRA745 Tool/software: Linux Hi Team,
we use Soc DRA745, 4G RAM, software build and download reference by http://omappedia.org/wiki/6AM.1.3_Release_Notes .
issue: out of memory. oom-killer was triggered, kill process again and agina till…
Hi Nick, "When building the Android filesystem, you are building the kernel before building the Android filesystem using these instructions, right?" ----Yes, first build kernel and uboot, second build android filesystem. Is the board at least getting…
You might try adding #pragma top of functions suspected to being overrun by CPU speed. The CCS simulator & emulator do slow code execution down quite a (bits) no pun intended. Assuming you have CLA section defined for code relocation into SRAM, you might…
Hi Paula,
I am sharing the log file:
DEBUG: Executing python function extend_recipe_sysroot
NOTE: Direct dependencies are ['/home/tisdk/tisdk/sources/oe-core/meta/recipes-core/glibc/cross-localedef-native_2.35.bb:do_populate_sysroot', '/home/tisdk…
Part Number: AM69 Tool/software: Hello TI Experts, We have custom hardware based on the AM69 SoC and intend to use the PCIE_SOC_REFCLK0_OUT, PCIE_SOC_REFCLK1_OUT, PCIE_SOC_REFCLK2_OUT, and PCIE_SOC_REFCLK3_OUT pins to provide reference clocks for PCIe…