Part Number: HD3SS214 Hi,
The datasheet specifies a max bandwidth of 8.1Gbps, but it's difficult to discern if the bandwidth is per channel or total across all 4 channels. This information would be really helpful.
Regards, Trinopoty Biswas
Part Number: HD3SS214 Hi,
I have question about HD3SS214.
Why don't need Ac-coupling capacitors on DCx(p), DCx(p) and AUXCx?
(mayby it's anarog SW, so DAx(p) or other capacitors works.)
Part Number: HD3SS214 Hi everyone,
We use the IC on a motherboard built around a COM Express module Type 6.
We have the following power states: G3, S5, S4, S3, S0.
As a reminder, G3 is mechanical off, S5 soft off, S4 suspend to disk, S3 suspend to RAM…
Part Number: HD3SS214 Hello,
I would like to correct my schematic. Please refer to the design picture below. The bottom part works via USB type C and the top part doesn't work. This is because I have AC coupling caps on AUX N/P lanes between the MXM card…
Part Number: HD3SS214 Hi Experts,
The customer wanted to confirm if the device functional modes described in chapter 7.4 of the datasheet and more particularly in table 7.1. was for both multiplexer and demultiplexer? The customer is using the IC as demux…
Part Number: HD3SS213 Other Parts Discussed in Thread: HD3SS214 , HD3SS215 Hi Team,
Customer is seeking HD3SS213ZQER 2nd source. The HD3SS214 and HD3SS215 are P2P solution with HD3SS213.
Could customer change HD3SS213 to HD3SS214/HD3SS215 without BOM changing…
Part Number: HD3SS214 Hi,
Are all of the DCx(p) and DCx(n) (where x = 0,1,2,3) all the same? With my board routing, I'll need to take the DP_ML_0 (p/n) diff pair and route it to DC3(p/n), DP_ML_1 (p/n) and route it to DC2(p/n) and so on.
Will there…