Part Number: HD3SS3202 Tool/software: I know how to calculate the internal junction temperature using the thermal resistances provided, but want to know what the maximum allowable operating temperature is.
Assuming 125°C, but wanted to confirm.
Part Number: HD3SS3202 Tool/software: Hello
I do have 2 questions:
1. do we have a device similar to HD3SS3202, however, with better crosstalk?
2. how is crosstalk in the datasheet defined / measured?
Thanks and regards
Alex
Part Number: HD3SS3202 Other Parts Discussed in Thread: TMUXHS4212 , Hi team,
do we have device to support below request?
Bidirectional 2:1 multi-channel differential signal multiplexer (functions are roughly shown in the figure below). The differential…
Part Number: HD3SS3202 Other Parts Discussed in Thread: TMUXHS4212 Hi,
I need to design a 4:1 USB 3.0 MUX ( without redriver , since it will be connected directly to a HUB).
Can I cascade 2x HD3SS3202 to do that?
We already use this part to do a 2:1 USB…
Part Number: HD3SS3212 Other Parts Discussed in Thread: HD3SS3202 Hello,
In another E2E thread, I saw that the insertion loss, cross talk, return loss, and off isolation specs are different between the two devices. However, when comparing the devices…
Part Number: HD3SS3202 Hi,
In OFF mode, I would like to use the VCC voltage of the HD3SS3202 is 0V.
I have two questions.
Q1:When I continue to use the HD3SS3202 with VCC=0V, is there damage to the HD3SS3202 ?
Q2:When VCC is 0V, are differential signal…
Part Number: HD3SS3202 Other Parts Discussed in Thread: TUSB542 , HD3SS6126 Hi
Because I am evaluating if it is possible to use HD3SS3202(MUX) to replace TUSB542(Redriver mux), I'd like to ask do you have any materials about this topic? Or what should…
Part Number: HD3SS3202 I designed USB TYPE-C using HD3SS3202.
I desigend schematic 1st picture, but TX line was twisted.
So I will swap the pins of A0p and A0n as shown in the 2nd picture. Is it possilbe methods?
A0p : USB3.0 TX - (negative) --------…
Part Number: HD3SS3202 Hi Team,
My customer is asking to confirm whether we have USB-IF certification or compliance test result with HD3SS3202 EVM.
Could you please help to confirm? Thanks.
Terry
Part Number: HD3SS3202 I designed USB TYPE-C using HD3SS3202.
I desigend schematic 1st picture, but TX line was twisted.
So I will swap the pins of A0p and A0n as shown in the 2nd picture. Is it possilbe methods?
A0p : USB3.0 TX - (negative) --------…