Part Number: HD3SS3202 Hi Team,
currently am design a PCB board and want to use HD3SS3202, but i cannot find the part on TI vault so i want the foot print or design files of the EVM so i can use it
Part Number: HD3SS3202 I have an application where there is a potential for the high speed signal lines to be shorted to ground. I need to know the maximum current rating of the high speed signal switches to make sure they don't get damaged during this…
Part Number: HD3SS3202 Other Parts Discussed in Thread: HD3SS3220 I already looked through every single post on TI's website regarding this device, tried all the suggestions and went through the recommended checklist but still can't seem to make it work…
Part Number: HD3SS460 Other Parts Discussed in Thread: HD3SS3212 , HD3SS3202 Hi,
I would like to use the HD3SS460 to cross-bar differential signals with the following properties:
Vcm = 1.8V +/- 10%
Vdiff = 1.5Vp-p +/- 10%
Rate = 500M
Can you please confirm…
Part Number: HD3SS3202 Hi Team,
I have a question about how PC recognize the speed of the MUX. Could you please help? Thanks!
For example, if the PC supports 10Gbps, when a type-c port with HD3SS3202 is connected to PC, how does the PC know if the type…
Part Number: TUSB322I Other Parts Discussed in Thread: HD3SS3202 , TUSB322 , HD3SS3212EVM , TUSB320EVM , TUSB320 , HD3SS3212 Hi team,
My customer would like to test the TUSB322 + HD3SS3202 combo.
I cannot find both of the EVMs, can you let me know what is…
Part Number: HD3SS3202 Other Parts Discussed in Thread: TS3USB221 , , TMUXHS4212 Hi HSSC team,
A key architect at Lab126 has requested a schematic review on the HD3SS3202 and TS3USB221 devices as per the attached. There are also additional questions as…