Part Number: HD3SS3412 One of my customer asked these questions below. Could you check them?
Is HD3SS3412 BUS-SW with differential signal?
Can this device do bi-directional communication?
Best regards,
Yuta
Part Number: HD3SS3412 Other Parts Discussed in Thread: HD3SS6126 Hi, I'd like to know if the HD3SS3412 switch is able to switch LVCMOS voltage level signals (3.3V max). I see that the device is rated for differential inputs of -0.5V to 4.0V, but is typically…
Part Number: HD3SS3412 Hi Sir
We have some question about HD3SS3412 want to check with you.
I check the similar question on TI E2E forum, the result in that discussion HD3SS3412 can work on 1000-base-T.
But here is a question want to check with…
Part Number: HD3SS3412 Other Parts Discussed in Thread: HD3SS3415 , Hi Team,
HD3SS3412 & HD3SS3415 These two differences?
I found these two can't see the difference, who can tell me their difference?
thanks
Kevin
Part Number: HD3SS3412 Dears
We have a customer who need a MUX for the CML signal, speed is around 3Gbps, and we would like to know if the HD3SS3412 can support?
Thanks
Jun Shen
Part Number: HD3SS3412HD3SS3412 is placed between the AURORA interfaces of the FPGA.
The AC coupling capacitor is located on the RX side. The bias on the TX side is within 2V.
The capacitor is placed at a different position from Fig. 11 in the data…
Part Number: HD3SS3412 Other Parts Discussed in Thread: TPS65988 Hi Sir,
The HD3SS3412 datasheet is show the SEL pull Low resistance 100k to GND.
and TPS65988 Evaluation Module show the SEL pull High resistance is 1k.
But our customer used 28…
Other Parts Discussed in Thread: HD3SS3412 , TMUXHS4212 Dear Sir,
1,Can use HD3SS3412 for 12G-SDI Switch? The BW of HD3SS3412 is 8 Gghz.But the datasheet said it can switch 12Ghz signal.
2,I also need fan-out device for 12G-SDI signal .Is ther any…
Part Number: HD3SS3412 Other Parts Discussed in Thread: HD3SS3411 , Hi Experts,
Do the HD3SS3412 and HD3SS3411 have a powered-off isolation feature? Basically, when 3.3V supply is off (no power to VDD or VCC), is Port A completely isolated from Port…