Hi Keegan, Steve ,
With multiple slave devices (as depicted in your drawing above). When cs[k] of device k is activated (goes low), transaction completes and cs[k] is automatically deactivates (goes high). For the k+1 device to be engaged in a transaction…
I have a custom board having TI8148 and I am trying to download the U-boot and Kernel images using JTAG through the SPI utility given in the PSP mentioned above. I am able to build the utility in ccs5.4 but when I am debugging it it is getting struck…
Hi,
I’m trying to do SPI booting of all the 8 cores of the C6678 using the MAD utilities, but it is not working.
Please help.
(Booting from 1 core is working fine – I am using the “spiboot” bat file (using hex6x)).
Problem description:
I am…
Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Hello,
I am using Serial Boot and Flash Loading Utility for OMAP-L13x evm based customized board.
The utilities works fine for small size of dsp*bin and appl*.bin but when the size dsp*.bin size…
Other Parts Discussed in Thread: ADS1298 , DM3730 Hi,
All genius:
In my project, DM3730 works as an SPI master in 8bit mode - the peer side is one sensor chip (TI ECG chip - ADS1298).
In my work system, DM3730 is running in wince 6.0.
The sensor…
Other Parts Discussed in Thread: HSADC-SPI-UTILITY , ADS5282 , ADS5282EVM Hi,
I recently got the ADS5282 EVM without the CD. I downloaded the ADC SPI software from: http://www.ti.com/tool/hsadc-spi-utility
But instead of installing the TI ADC SPI…
I have been searching through TI's DSP-BIOS, GPIO and SPI documents looking for a way to adjust drive strength on the SPI lines, but have come up empty. Does anyone know if this is even software adjustable?
Thanks,
- Jonathan
Hi,
the SPI GUI installer version 5.1 is now active again at that location http://www.ti.com/tool/hsadc-spi-utility . you could now download that GUI and control the ADS5562 EVM, but with the same caveat as I mentioned before that the installer was…
Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 I followed the instructions in http://wiki.davincidsp.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L138 to flash the SPI flash on the OMAPL138 experimenter board. I tried flashing the…
Thanks, Richard.
There is no any CD or a memory stick in ADS EVM shipping box.
I could find the SPI installer (ver. SPI 5.1)at the following link:
I have some more questions on SPI software.
1) If there is a manual for SPI software, please…