Part Number: TPS2419 Hi
My customer is using TPS2419 to combine 1 1 redundant power supplies. when these two power supplies are working, there are whistlers from power supplies. If we turn off any of them, the whistlers will disappear. The specifications…
Dear Ti E2E community
Am facing the clock drift issue when I run the below attached app, it says that sound card is facing clock drifts, but I don't see this issue in ti sdk 7, could you please try to reproduce this issue from your end & let me know…
Yan Liu said: Does this mean that these two values are still not large enough?
We have seen that happen, can depend on unpowered breakaway torque of rotor magnets to stator laminations. Check the lock rotor flag is not enabled at any point for SPM or…
Part Number: TDA4VM
Tool/software:
Hello,
We are trying to run out model on EdgeAI 9.20.07 . https://github.com/TexasInstruments/edgeai-tidl-tools/tree/09_02_07_00?tab=readme-ov-file .
We have observed issue with Matmul layer on target when…
Hi,
We are using the SK-AM62 E3 revision. Can you please confirm which revision are you testing the HDMI audio?
Shorted the j24 pins. Still HDMI audio is not coming.
Attached the boot logs for you.
Fullscreen
5367.Bootlog.txt
Download…
Part Number: TDA2 Tool/software: TI-RTOS Hello, I'm running the TIDL object detection usecase, and usecase is running fine only with a small problem here:
My original input file is .MP4 with resolution 1920*1080, and I make it to .h264 with resolution…
Hello Ananya,
Please find the details which you asked over the meeting below. awr2944_corner_radar_Debug.appimage.txt awr2944_corner_radar_mss.xer5f.txt awr2944_corner_radar_dss.xe66.txt Let us know if you need more infomration Regards,
Ritu
Hi user4016414,
I'm attaching a zip file which contains an http client example for 6748. Hopefully you can pull something out of this to add to your http server.
8015.ndk_evm6748_elf_client.zip.txt
Best regards,
Janet
Could you please try the following:
1. Download the file attached. Change the extension from .txt to .bin
2. Run it from the command line with the following parameters:
"ti_simpack_vayu_ccs_0.6.2.0_setup.bin" --mode silent --prefix "/home/vasanthaangappan…