Part Number: ISO5452-Q1 Other Parts Discussed in Thread: ISO5452 Hi Ti,
I am performing short circuit type -1 test based on AQG324 standard. I am using an external wire to short the High side switch and using a function generator to give gate pulse…
Part Number: ISO5452-Q1 Other Parts Discussed in Thread: ISO5452 Tool/software: WEBENCH® Design Tools Hello,
Need your immediate support
I downloaded unencrypted spice model of ISO5852SDW for ISO5452. I am working in Simetrix which can support this…
Part Number: ISO5452-Q1 Other Parts Discussed in Thread: ISO5452 , UCC21750 您好,
想问下,ISO5452芯片是否有软关断功能丢失的情况?从Datasheet得知,desat触发阈值时,芯片阻断输出,将OUTL拉至低电平持续2us。而实际结果是只有600ns左右,相比正常的关断时间只多了200ns左右。如图所示:黄色CH1通道为desat脚外部电容充电,蓝色CH2为芯片门极输出,触发阈值后,门极输出下降时间为600ns左右…
Part Number: ISO5452-Q1 Hi Team,
Either UVLO1 or UVLO2 occurs, the RDY pin output goes low. What about the FLT Pin behaviors under UVLO1 or UVLO2?
And when desaturation is active, the RDY will go low and then go high, does this design to prevent FLT…
Part Number: ISO5452-Q1 Other Parts Discussed in Thread: TINA-TI , , ISO5451 Tool/software: TINA-TI or Spice Models Hi,
Could you please send me the Pspice Model of ISO5452-Q1, wayne.liu@ti.com Thanks.
Hi Grant,
Thanks for your interest in ISO5452-Q1. I'm an applications engineer in the high power drivers group and can help answer your question.
I also can't find any zeners which have their listed knee at the 0.5-mA desat charge current. Looking…
Part Number: ISO5452-Q1 Hi,
My customer would like to connect RDY and FLT together to save MCU GPIO, so in this case, when FLT is set to 0, can we pull RST low and make FLT goes back to high and the chip goes back to normal? Because Datasheet Figure…
Part Number: ISO5452-Q1 Other Parts Discussed in Thread: ISO5452 , UCC21520 Hello,
For the ISO5452, can I drive the RESET pin with an active low signal to disable the outputs? I have windowed comparators that trigger for overcurrent events on the 3…
Part Number: ISO5452-Q1 Hello, Is it fine to add pull up to the DESAT, to increase the current flow to get a lower over current detection limit? Best regards, Anton