Part Number: ISO5852SEVM Hi team,
Can you tell us the external size of the EVM? Also, if you have a pdf file that shows it, please send it to me.
Sincerely, Ryu.
Part Number: ISO5852SEVM Other Parts Discussed in Thread: UCC21750 , TIDM-1000 , ISO5852S I'm new to designing high power electronics and want to start doing so with IGBT's. I need to design a active front end or PFC( AC to DC converter). I'm finding…
Luis,
Yes, EVM can be used with the parameters you need. We recommend the EVM for use in evaluating the ICs only. Note that the speed of the turn-on and turn-off pulses on output is dictated by external gate resistor and the load (your IGBT/Mosfet gate…
Luis,
The thread is here:
https://e2e.ti.com/support/power-management/f/196/t/918908
Can we stick on the thread above, its harder to follow if the replies will be split in 2 threads.
best
dimitri
Part Number: ISO5852SEVM Hello E2E,
www.tij.co.jp/.../sllu298.pdf The characters of EVM schematic is cloudy. I can't read them. Does TI have vivid schematic?
Regards, ACGUY
Part Number: ISO5852SEVM On the ISO5852SEVM, what’s limiting the Vdc to go over 500V? Is it the TO-220 package through holes?
Can you please share the layout of the board in PDF?
Other Parts Discussed in Thread: ISO5852SEVM , ISO5852S , TIDA-00195 Hi,
I have a task to develop a multi-channel power controller. It have to control temperature in the IR oven. The source of the control signal is a controller and the driver - ISO5852…