Part Number: ISO6721-Q1 Hey Team,
I have a few questions regarding the ISO6721-Q1's use in a system where the measured voltage can change very slowly (millihertz range).
1. Is there any issue with holding the input between threshold states (For seconds…
Part Number: ISO6721-Q1 Hi team,
the device has "Wide supply range: 1.71 V to 1.89 V and 2.25 V to 5.5 V".
why the device dos not support supply voltage :1.89V to 2.25V? is there any reason?
best regards,
Kazusa suzuki
Part Number: ISO6721-Q1 Hello Team,
My Customer is working with XISO6721FBQDRQ1 and wondering if they have to use a digital isolator with "default high" or "default low" to isolate their RXD TXD signals from CAN Transceiver?
Regards…
Part Number: ISO6721-Q1 Hi team,
Does "2 mm maximum from VCC1" shown in "Layout Example" mean that 0.1uF must be within 2mm away from VCC1 pin? I guess that the closer to VCC1 0.1uF capacitor is, the better layout or noise performance…
Part Number: ISO7421E Other Parts Discussed in Thread: ISO7721-Q1 , ISO6721-Q1 , , ISOW7841 , ISOW7741 , SN6505B , ISO7741-Q1 , ISOW7741-Q1 Dear team,
I am looking for the digital isolator of automotive grade with 2.5kv ISOLATION and found this part ISO7421EQDWRQ1…
Part Number: ISO6721R-Q1 Other Parts Discussed in Thread: ISO6721R , ISO6721 Hi,
Whats the difference between ISO6721RB-Q1 and ISO6721B-Q1
It seems non R version is reinforced isolation, so why R version is not reinforced? What does the R stand for so? …
Part Number: ISOW7841A-Q1 Other Parts Discussed in Thread: ISO6721 , ISO7721 , ISO6521 , ISOW7741 , ISOW7721 , ISOW7821 Hello team,
I kindly request you to please provide the PN suggestion for GND isolation. ISOW7841FAQDWERQ1 is a device which has higher specs…
Part Number: AM2634 Other Parts Discussed in Thread: TCAN1044-Q1 , ISO6721 Hi team,
My customer is planning on using AM2634 in their new design, where they will use CAN wake up function to wake up the PMIC before putting the MCU in working state.
For this…
Part Number: TINA-TI Other Parts Discussed in Thread: ISO6721 , ISO7721 , ISO6721-Q1 , I was trying to insert ISO6721 and ISO7721 Spice model into TINA through macro wizard tool but I was getting the following DBREAK error.
Kindly help on this. Thanks in…
Part Number: ISO1640-Q1 Other Parts Discussed in Thread: ISO7721-Q1 , ISO6721-Q1 , , ISO6721 , ISO7721 , ISO1640 Hello team,
My customer is looking for UART isolator.
I cannot recommend digital isolator such as ISO6721-Q1, ISO7721-Q1 because customer wants…