Hi Hassan,
Thanks for reaching out.
The device has been characterized for the datarates specified in the datasheet, i.e., at 0 Mbps and 25 Mbps. We do not have characterization data for 9 Mbps but we expect it to be between 11mA and 17mA, as you would…
Hi Glen,
Thanks for reaching out and for your interest in ISO7331C.
I understand the component shortage has made it difficult for most customers. Unfortunately, the datarate and power supply operating voltage are two different parameters and not necessarily…
Part Number: ISO6742 Other Parts Discussed in Thread: ISO6721 , , THVD1500 , ISO6721R , ISO6731 , ISO6741 , ISO1500 , ISO1430 , ISO1450 , ISO1410 Hi experts,
My customer want to realize isolated RS485 through using ISO6742 and THVD1500. But, from my opinion, the…
Part Number: ISO7731 Other Parts Discussed in Thread: ISO6731 , ISO7831 The creepage distances of ISO7731 and ISO6731 Only 8mm, it cannot meet customer demand that is 11.5mm creepage distances, so I would like to ask if there is an isolation plan that…
Quickly find solutions to common questions about digital isolator devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
FAQ: Isolation >> Digital Isol…