Part Number: ISO7741 Other Parts Discussed in Thread: ISO6741-Q1 Tool/software: Dear team,
I would like to use digital isolator for SPI communication with ADS1018IDGST. can you please suggest/recommend which series of isolater will be good for this…
Part Number: ISO7041-Q1 Other Parts Discussed in Thread: ISO7041 , ISO6741-Q1 We plan to use the digital Isolator ISO7041-Q1 – and / but we need a supply voltage of 1.8V.
On the TI-webpage we can search/filter for digital isolators with 1.8V and the…
Part Number: ISO7341-Q1 Other Parts Discussed in Thread: ISO6741-Q1 We have built some boards using the ISO7341CQDWQ1 chip. Due to an error, the bypass caps are 1.0uF instead of the 0.1uF in the data sheet. Should this cause any problem?
Part Number: ISO7241C-Q1 Other Parts Discussed in Thread: ISO7741-Q1 , ISO6741-Q1 Hello,
I wanted to know the difference between the ISO7241 automotive variant (AECQ certified) and industrial variant. I saw in the QRP packaging datasheet that the amount…
Hi Garam:
Thanks for posting your question on E2E!
Our latest general purpose isolator, ISO6741-Q1 , is a P2P with ISO7741-Q1. In addition, most of our 4-channel older generation isolators are P2P with ISO7741-Q1.
Are there any other key specifications…
Part Number: UCC28740-Q1 Other Parts Discussed in Thread: UCC28730-Q1 , ISO7741-Q1 , ISO7710-Q1 , ISO6741-Q1 , ISO6721-Q1 , , SN6505B-Q1 Hi team,
Do you have any cost-effective automotive grade optocoupler recommendations? It seems Vishay is the only…
Hi John,
Thanks for reaching out.
I understand you are looking for a digital isolator that offers VIOWM of 4-5kV DC. Generally, the VIOWM is based off of the dielectric breakdown time. This means that the working voltage is based on a lifetime of…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6721 , ISO6741 Hi team,
As we know,ISO7221 is TTL input type and ISO6721 is CMOS input type. Do you have any suggestion on the compatible design on these two device?
ISO6721 input voltage…
Part Number: TLIN2021A-Q1 Other Parts Discussed in Thread: ISO6731 , ISO6741 , TMUX7219-Q1 Hi,
See I have one master and two slaves, some time one slave switch to master that time I need to isolate main master. Is there any possible way to isolate main…
Part Number: ISO7341-Q1 Other Parts Discussed in Thread: ISO7741 , ISO7710 , ISO6741 Dear team,
Can you please help to share the comparison table of ISO7341FCQDWRQ1 & ISO7710FQDWRQ1? Thank you for your help in advance.