Part Number: ISO6742-Q1 Hi Team,
I'm using the isolator ISO6742QDWRQ1 in my board.
Please find the attached schematics and provide the feedback.
ISO6742QDWRQ1 - DIO isolator.pdf
Regards,
Abhishek
Part Number: ISO6742-Q1 Other Parts Discussed in Thread: ISO7842 Tool/software: Hi,
Would you please suggest what is meaning of the below option 01/02/03? does it mean we can choose any one of the setting?
Why for same package, ISO7842FDWWR , there…
Part Number: ISO6742-Q1 Other Parts Discussed in Thread: ISO6742 Tool/software: Hello Team,
What is the maximum input clamping current of the isolator ISO6742?
Besides, why are there two sets of input clamping diodes on each input? What is the…
Part Number: ISO6742-Q1 hello,
I have one question regarding the EN PIN of the ISO6742-Q1 that whether the EN could connect to VCC directly or need a current limited resistor?
Thanks for your support!
Other Parts Discussed in Thread: ISO6742 , SN74LVC1G125 Tool/software: Hello ,
We have a digital bidirectional pin which has to isolated using ISO6742D , Is below configuration is fine to use ? (We already have ISO6742 in our design and want to use…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO6742-Q1 Tool/software: I want to design a gate driver module for a 2.3kv Sic modules. Isolation requirement (reinforced isolation) is given below;
Material Group : 1 Pollution Degree : 2 Altitude…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO7242C , ISO6742-Q1 , ISO7741-Q1 Tool/software: Hi,
A my account is search for a P2P compatible device with NSi8242W-DSWR which supports TTL input signal. The input voltage threshold of ISO7842…
Hi Tom,
Please see attached the updated UL certificate. It lists ISOM8111 (DFS package) at 5000 Vrms.
I'll be posting this certificate online within the next month.
Thanks, Saleem Marwat
UL Certificate of Compliance File E181974 Vol 4 Sec 6.p…
Part Number: P82B96 Other Parts Discussed in Thread: ISO1640 , ISO1640-Q1 , P82B715 , ISO6742 , ISO7742 Hi, I'm using the P82B96 for a simple I2C extender, but I am not reading anything on the TXRX or TYRY. I've tried increasing the 3.3V that pull up…
Part Number: BQ75614-Q1 Other Parts Discussed in Thread: TXS0102 , ISO6742 Hi,
on our BQ75614EVM as well as in a couple of other threads, we recommend using ISO7342 on UART connection between MCU and BQ75614:
- why do we recommend an isolation instead…