Other Parts Discussed in Thread: ISO7220B Hi, I have a 1MHz clk signal generated by MSP430 with VH=3.6V, VL=GND. I want to change the clock signal to the one with VH=2.5V and VL=-2.5V. Based on the datasheet of ISO7220B, it seems OK to fulfill this translation…
Conor,
I will work to get answers on the above, but our systems and product teams are still largely out for the holiday, so it may take some time to run this down.
As far as I am aware. I do not believe we have a published certificate specifically…
Part Number: UCC23513 Hi,
What is the UL number of UCC23513DWYR? Is it number for 20190711-E181974 on the attached file?
Please help to confirm it. Thanks!
sluq004-ucc23513.pdf
Hi Brian,
Attached is a document which covers what Texas Instruments devices have UL1577 certification as of 6-18-2024. The latest document can be found on the UL website.
In this document you can see the TPSI3052-Q1 covered.
UL1577.pdf
Best Regards…
Hello Mitesh,
Thank you for reaching out to our team's E2E.
You can find the UL certificate for TPSI2072QDWQRQ1 on the UL website at the following link: FPPT2.E181974 - Nonoptical Isolating Devices - Component | UL Product iQ
For your convenience…
Other Parts Discussed in Thread: ISO7140CC The data sheet (and the design guide) for the ISO71xxCC 4242-VPK Small-Footprint Low-Power Triple and Quad Channels Digital Isolators references a carrier frequency used for PWM of low frequency (<100kHz) inputs…
Other Parts Discussed in Thread: TXS0108E , ISO7242C , SN74AVC2T245 I am working on bidirectional, isolated Digital I/O, which can be used as I2C or SPI. Each one DIO channel has to have full configuration flexibility (input or output, work with output…
Hello Kazuya,
I've attached the certification documents. Additional information about the test method can be found on the UL or VDE website.
In the future, the latest revision of these document should be available under "Technical Documentation" on…
Hi Hyejeong,
These devices have already completed certification. The datasheet update is in progress, but I do not have a firm date to provide. Please see attached certifications for these devices.
E181974-Vol4-Sec6-20260312_CoC.pdf E181974-Vol4-Sec1…