Part Number: ISO7240M Other Parts Discussed in Thread: UCC27714EVM-551 , , ISO6440 Hi team,
Our customer is currently evaluating the UCC27714EVM-551 evaluation board. This board is populated with the ISO7240M.
On this board, when the secondary-side…
Part Number: ISO7240M Other Parts Discussed in Thread: ISO6440
Dear Support Team,
We are using the ISO7240M in our system.
A customer reported an output malfunction, and our investigation revealed that the signal fails to propagate correctly when…
Part Number: ISO7240M Hello, My customer would like to use ISO7240M as an isolated clock buffer, in/out are not data stream, they are just fixed 100MHz clock. In this case, how much additive jitter does TI think would be added? Best regards, K.Hirano
Part Number: ISO7240M Tool/software: Hello team,
The datasheet states 200Mbps as TYP and 150Mbps as MAX data rate.
Shouldn't it be the other way around?
Best Regards, Kei Kuwahara
Part Number: ISO7240M Other Parts Discussed in Thread: ISO7740 , , ISO7240CF
Tool/software:
Dear Technical Support Team,
Unexpected momentarily glitch(about 2.5V , 8us) on the output during power up, at a time when Vcc2 is at about 2.5V.
See attached…
Part Number: ISO7240M
Good afternoon,
I have a question, there found two differences on the edge of this this part(different Mfg Lot).
Need some help to confirm on this component edge because in datasheet only available for "bevel edge".
Or else…
Part Number: ISO7240M Other Parts Discussed in Thread: ISO7740 Good afternoon. We have product ISO7240MDWR, there is marking:
OCCE HCT ISO7240M G4
Will you please give me the date of production of the TI product. Thanks for your help.
Part Number: ISO7240M Other Parts Discussed in Thread: UCC28950 , TINA-TI , Hi,
I am working on phase-shift full-bridge converter, and for that, I want to use isolator ISO7240 to drive 4 MOSFET on the primary side of the transformer (controller UCC28950…
Part Number: ISO7240M Hello support team,
I have some questions regarding "VIORM: Maximum repetitive peak isolation voltage" of ISO72xx series. This specification is specified with AC voltage.
[Questions] 1. How much is the frequency of this AC voltage…
Other Parts Discussed in Thread: ISO7240M , ISO7340C , ISO7640FM , ISO7840 Hello, Could you please let me know the maximum supply current of ISO7240M at the following conditions? -Data Rate : 90Mbps, 50Mbps, 25Mbps -Vcc1=Vcc2=5V I promoted the ISO7240M…