Part Number: ISO7420E We have noticed a behavior in several of our devices that we cannot explain 100%. We have a serial data link with four signals routed via two ISO7420ED. Both isolators are supplied by the same voltage. They are directly next to each…
Part Number: ISO7420 Other Parts Discussed in Thread: ISO1211 , ISO224 Are there any isolators that allow up to 12 V supply voltage and pin compatible with ISO7420?
Thank you
Other Parts Discussed in Thread: TPS28226 , ISO7420 , ISO7820 , ISO7320C , ISO7720 , ISO7740 Hi! I want to generate pwm signal for the mosfet's gate of a buck converter, and i'm generating the pwm signal from a fpga. I need to protect my fpga, so i'm going to…
Other Parts Discussed in Thread: ISO7420 HI
When I'm looking into datasheet for ISO7220/21A and compare it with data from ISO7420/21 I'm not understand where ISO722x have benefit compare with ISO742x.
Both have the same datarate 1Mbps and same…
Need data on current consumption for ICC2 based on characteristics of load capacitance and signal frequency. Something more in-depth than what is in data sheet.
Hi Eric, Thank you for posting, and welcome to E2E! The POR for ISO7420 detects when voltage is below its ~3V threshold, and the corresponding outputs become high-impedance (Hi-Z) instead of HIGH or LOW. When local power is not present on the output power…
Hi Anand,
Customer tried only ISO7420 about noise insertion test.
Customer wants to consider whether this issue occur with ISO7720 or not.
In addition, Customer is considering the mechanism of issue at ISO7420 now.
This issue has been resolved by adding…
Part Number: UCC28950 Other Parts Discussed in Thread: PMP6712 , UCC21520 , ISO7420 Hi Expert,
The customer would like to run 2pcs UCC28950 in parallel.
They want to know why PMP6712 design locate the UCC28950 at primary side?
Any particular reason here…
Part Number: LM5045 Other Parts Discussed in Thread: UCC2897A , ISO7420 Hi! Ti E2E,
My application is wide input voltage (30 to 120) VDC to 48VDC output. I wonder whether I can use LM5045/46 for this application. (It must have boost and buck function…