Part Number: ISO7421 Other Parts Discussed in Thread: ISO7720 , ISO7761 , ISO7741 , ISO1410 Hi everyone,
I'm looking for a replacement for IL711 isolator, but I have few questions
Can I use "Capacitive Coupling" technology instead of GMR (Giant…
Part Number: ISO7421 Other Parts Discussed in Thread: ISO7721 , ISO7321C Dear Sir or Madame,
We are developing a wearable product for biomedical purposes, which transfers data to and from the host through a UART interface, at 115200 bauds. In order to…
Part Number: ISO7421 Other Parts Discussed in Thread: ISO7721 What is the frequency of the internal oscillator used for low frequency signals? I am putting 24 of these in a piece of equipment and don't want issues passing FCC EMI tests. Thanks,
Part Number: ISO7421 Other Parts Discussed in Thread: ISO7721 hi dear supporting team,
customer is sourcing for low cost digital isolator, the spec requirement is as below, it seems the closest solution on site areISO7421, but it is high rel, so do we…
Part Number: ISO7221C-HT
hi dear supporting team,
customer is sourcing for low cost digital isolator, the spec requirement is as below, it seems the closest solution on site areISO7421, but it is high rel, so do we have newer ones with lower cost?
1…
Part Number: ISO7421 Dears,
Our customer is using ISO7421 in his design. He had done a EFT burst test, but it failed. The test condition is 1kV, 5kHz, 1 minute. Does this device could bear 1kV EFT burst? If couldn't, kindly suggest some methods to solve…
Part Number: ISO7421 Hello Team,
I need to isolate a bipolar supply of +/- 3 V from a 3.3-V signal. This means that the common-mode voltage between GND1 and GND2 would be 3 V. Would this work? Is this allowed (abs-max) with any of the digital isolators (such…
Part Number: ISO7421 Other Parts Discussed in Thread: ISO7721 Hi,
My railway customer wants to do the safety analysis, two questions:
1. What is the possibility of input and output short? In what conditions the short will happen?
2. If the isolation voltage…
Other Parts Discussed in Thread: ISO7421 , ISO7321C Hi There
I am looking at replacing our H/S optocouples with an ISO7421 as we require a feedback path but require some extra information.
We are using the "opto" to send/receive high precision IRIG-B data…