Part Number: ISO7741 Other Parts Discussed in Thread: ISO7641FM , ISO7241M , ISO7821LLS Is there any device able to compete with MAX14131? customer need speed up to 150Mbps for VFD application. thanks.
Hi Robert ,
Thanks for posting your question on our forums. [ Alex , quick thank you for your responses as well!]
We do have devices with < 1ns jitter if that is still of interest. For example, the ISO7641FM can do 0.5ns. Please see Figure 14 below [taken…
Other Parts Discussed in Thread: ISO7641FM , ISO7841 Hi Expart. I need information about Surge immunity of ISO7641FM.
In ISO7841, datasheet[Page.5] says the following.
"Surge immunity 12.8kV[MAX]" www.tij.co.jp/.../iso7841.pdf
Please tell me Surge…
Hi Ted,
Did you mean to say ISO7641FM is taking 3mA of input current? Or did you mean you want the device to take at least 3mA of input current?
ISO7641FM only requires a maximum of 10µA as input current and it doesn't take anything more than 10µA even…
Other Parts Discussed in Thread: ISO7641FM hello,
I am using DS92lv1021/1212 SERDES for lvds serial communication. Signals inclusing clock (TCLK, REFCLK) to SERDES ic are provided through ISO7641FM. I am operating SERDES at clock rate of 16 MHz.
My question…
Hell Joseph-san
Customers should test confirmation, thank you.
This is the question the background but, from the drive capacity of ISO7641FM, I wanted to check if you can drive the CLK and SCLK of ADS1252U to be used for load.
Think has circuitry
ISO7641FM…
Other Parts Discussed in Thread: ISO7631FM , SN65HVD37 , ISO7641FM Hello, all
Now we have one inquiry regarding internal isolation distance on ISO7631FM from our customer.
Please refer to the item below, and feedback us with your comment.
Now we are looking…
Hello Raul,
our test engineers have the following suggestion:
Since the issue is occurring during high dV/dt it may be the ISO7641FM is responding to transient energy coupling onto inputs given the ISO7641FM does not have input filters.
Hence, could you…
Other Parts Discussed in Thread: ADS1158 , AM3352 , ISO7641FM Hi all,
In one of our designs, we have used ADS1158 to measure the 8 analog inputs.
We have configured ADC in Auto Scan mode with 8 channels enabled.
The set data rate is 1075 SPS , thus the sampling…
Quickly find solutions to common questions about digital isolator devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
FAQ: Isolation >> Digital Isol…